How to create flash.bin on i.MX8M with DDR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to create flash.bin on i.MX8M with DDR3

2,673 Views
muhualuo
Contributor II

Hi ,

I'm using DDR3L on i.MX8M,  I have put two files(ddr_init.c and ddrphy_train.c) to my uboot-imx project ,and compiled success, generated  u-boot-nodtb.bin  and spl/u-boot-spl.bin ,but I don't know how to create flash.bin.

I read the standalone build  guide (i.MX8M Standalone Build.pdf),but it only described lpddr4, No DDR3 involved.

pastedImage_1.png

I need to generate DDR3 image(flash.bin),  how to operate ?

thanks

Muhua Luo

0 Kudos
Reply
1 Reply

2,431 Views
igorpadykov
NXP Employee
NXP Employee

Hi Muhua

one can use uboot/configs/imx8mq_ddr3l_arm2_defconfig,

building steps can be found in Yocto Guide included in linux documentation on
i.MX Software | NXP 

or third party tutorials

https://developer.solid-run.com/knowledge-base/i-mx8m-atf-u-boot-and-linux-kernel/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply