How to control the USB_OTG_PWR and the USB_H1_PWR of i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to control the USB_OTG_PWR and the USB_H1_PWR of i.MX6

ソリューションへジャンプ
2,998件の閲覧回数
yuuki
Senior Contributor II

I understand that USB_OTG_PWR and USB_H1_PWR are the signals which control each VBUS of USB OTG and USB Host1.

These signals are assigned to the following pins.

- USB_OTG_PWR : EIM_D22(ALT4) or KEY_ROW4(ALT2)
- USB_H1_PWR : EIM_D31(ALT6) or GPIO_0(ALT6)
"To control PMIC to supply VBUS voltage"

However, I cannot find the register bit filde for controlling these signals.
Could you teach register bit filde which controls these signals?

Best Regards,

タグ(3)
0 件の賞賛
返信
1 解決策
2,167件の閲覧回数
alfred_liu
NXP Employee
NXP Employee

Hi, YUuki

these two signals are just alike normal GPIO, no special register for USB_OTG_PWR and USB_H1_PWR.


元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,167件の閲覧回数
alfred_liu
NXP Employee
NXP Employee


Hi, Yuuki

consulted with BSP team.

they treated these two signals as normal GPIO in linux till now.

2,168件の閲覧回数
alfred_liu
NXP Employee
NXP Employee

Hi, YUuki

these two signals are just alike normal GPIO, no special register for USB_OTG_PWR and USB_H1_PWR.


0 件の賞賛
返信