How to connect SRAM with 16bit bus in imx6sx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to connect SRAM with 16bit bus in imx6sx

397 次查看
hyoungkikim
Contributor IV

Hi all
i am not good at English , please understand

I'm trying to connect an external SRAM with 16 bits using i.MX6SX. In the old CPUs, when connecting a 16bit device, the A0 of the device was connected to A1 of the CPU with Byte Enable pin as A0, because CPU is 8 bit bus and a device is 16 bit bus . However, I heard that ARM CPUs have internal bus and external bus and they are different , and the A0 PIN is connected to internal A0 or internal A1 depending on the bus width which defined in chip select configuration .

so when i connect 16bit SRAM , i will connect CPU A0 PIN to the device A0 with Byte Enable
Is that correct?

标签 (2)
标记 (1)
0 项奖励
回复
2 回复数

369 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @hyoungkikim ,

Your understandings are right.

Note:

AD0~AD15 are used as address lines, D16~D31 are used as data lines.

Hope this can do help for you

Wish you have a nice day

Best Regards

Rita

0 项奖励
回复

374 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

I will help check it , please wait.

0 项奖励
回复