Hi all
Let me confirm about the connection of EIM for i.MX6SL.
My customer plan to boot from NOR-SPI flash(16bit).
In that case, is the above connection correct ?
P.S.
I refer to the following link.
https://community.nxp.com/message/437106
Ko-hey
Hi Ko-hey
it is correct with left column should be AUS=0 Address shifted according to port size,
connecting the address signals one to one (for example, A0→A0 and A1→A1).
and right column should be AUS=1.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
Is following table correct ?
AUS=0 | AUS=1 | NOR | |
ADDRESS | EIM_ADDR[22] | EIM_ADDR[23] | A[22] |
EIM_ADDR[21] | EIM_ADDR[22] | A[21] | |
EIM_ADDR[20] | EIM_ADDR[21] | A[20] | |
EIM_ADDR[19] | EIM_ADDR[20] | A[19] | |
EIM_ADDR[18] | EIM_ADDR[19] | A[18] | |
EIM_ADDR[17] | EIM_ADDR[18] | A[17] | |
EIM_ADDR[16] | EIM_ADDR[17] | A[16] | |
EIM_AD[15] | EIM_ADDR[16] | A[15] | |
EIM_AD[14] | EIM_AD[15] | A[14] | |
EIM_AD[13] | EIM_AD[14] | A[13] | |
EIM_AD[12] | EIM_AD[13] | A[12] | |
EIM_AD[11] | EIM_AD[12] | A[11] | |
EIM_AD[10] | EIM_AD[11] | A[10] | |
EIM_AD[9] | EIM_AD[10] | A[9] | |
EIM_AD[8] | EIM_AD[9] | A[8] | |
EIM_AD[7] | EIM_AD[8] | A[7] | |
EIM_AD[6] | EIM_AD[7] | A[6] | |
EIM_AD[5] | EIM_AD[6] | A[5] | |
EIM_AD[4] | EIM_AD[5] | A[4] | |
EIM_AD[3] | EIM_AD[4] | A[3] | |
EIM_AD[2] | EIM_AD[3] | A[2] | |
EIM_AD[1] | EIM_AD[2] | A[1] | |
EIM_AD[0] | EIM_AD[1] | A[0] | |
DATA | LCD_DAT[21] | LCD_DAT[21] | DQ[15] |
LCD_DAT[20] | LCD_DAT[20] | DQ[14] | |
LCD_DAT[19] | LCD_DAT[19] | DQ[13] | |
LCD_DAT[18] | LCD_DAT[18] | DQ[12] | |
LCD_DAT[17] | LCD_DAT[17] | DQ[11] | |
LCD_DAT[16] | LCD_DAT[16] | DQ[10] | |
LCD_DAT[15] | LCD_DAT[15] | DQ[9] | |
LCD_DAT[14] | LCD_DAT[14] | DQ[8] | |
LCD_DAT[13] | LCD_DAT[13] | DQ[7] | |
LCD_DAT[12] | LCD_DAT[12] | DQ[6] | |
LCD_DAT[11] | LCD_DAT[11] | DQ[5] | |
LCD_DAT[10] | LCD_DAT[10] | DQ[4] | |
LCD_DAT[9] | LCD_DAT[9] | DQ[3] | |
LCD_DAT[8] | LCD_DAT[8] | DQ[2] | |
LCD_DAT[7] | LCD_DAT[7] | DQ[1] | |
LCD_DAT[6] | LCD_DAT[6] | DQ[0] |
Ko-hey
Hi Ko-hey
yes correct
Best regards
igor