How to connect DDR3L to i.MX6 ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to connect DDR3L to i.MX6 ULL

1,374 Views
michaelnübling
Contributor I

Can you please tell me how to connect two DDR3L chips of 256MByte density and a 16bit wide data bus to a i.MX6 ULL processor?

Labels (1)
0 Kudos
5 Replies

1,196 Views
michaelnübling
Contributor I

Hi Igor,

thanks for your answer. I have these design files but I am still not sure how to connect two DDR3L chips to the i.MX6 ULL. In the schematic the schematic I can only find one chip connected to the i.MX6 ULL with the option to connect a twin- die DDR3L to the i.MX6 ULL.

Can I connect two chips instead of one twin-die chip just using the signals ODT1,SDCKE1, ZQ1 and CS1?

I am a little bit confused because in the Reference Manual for the i.MX 6ULL processor on page 2218 I found this Note:

NOTE
This feature will not be supported for DDR3 since only a single
chip select is supported for DDR3

Can you explain this to me?

Best regards

Michael

0 Kudos

1,196 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michael

seems this statement was left from i.MX6SX Reference Manual,  i.MX6SX
works fine with ddr3  two chip selects.

Best regards
igor

0 Kudos

1,196 Views
michaelnübling
Contributor I

Hello Igor,

thanks for your answer,

I have one more question.

On page 2276 of the reference manual I can find the information that

address mirroring will only work for DDR2/DDR3 memories and not for

DDR2L/DDR3L. Is this right?

(Embedded image moved to file: pic01200.gif)

Mit freundlichen Grüßen

i. A. Dipl.Ing.(FH) Michael Nübling

Hardwareentwicklung

S. Siedle & Söhne Telefon- und Telegrafenwerke OHG

Bregstraße 1, 78120 Furtwangen

Telefon: +49 7723 63-307

Von: "igorpadykov" <admin@community.nxp.com>

An: "Michael Nübling" <michael.nuebling@siedle.de>

Datum: 15.05.2018 14:20

Betreff: Re: - Re: How to connect DDR3L to i.MX6 ULL

NXP Community

Re: How to connect DDR3L to i.MX6 ULL

reply from igorpadykov in i.MX Community - View the full discussion

Hi Michael

seems this statement was left from i.MX6SX Reference Manual, i.MX6SX

works fine with ddr3 two chip selects.

Best regards

igor

Reply to this message by replying to this email, or go to the message on

NXP Community

Start a new discussion in i.MX Community by email or at NXP Community

Following Re: How to connect DDR3L to i.MX6 ULL in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email

frequency in your email preferences

0 Kudos

1,196 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michael

please look at i.MX6ULL EVK design files

Schematics (1)
Design files, including hardware schematics, Gerbers, and OrCAD files.
MCIMX6ULL-EVK_DESIGNFILES
http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/ev...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,196 Views
michaelnübling
Contributor I

Hi Igor,

thanks for your answer. I have these design files but I am still not sure

how to connect two DDR3L chips to the i.MX6 ULL. In the schematic the

schematic I can only find one chip connected to the i.MX6 ULL with the

option to connect a twin- die DDR3L to the i.MX6 ULL.

Can I connect two chips instead of one twin-die chip just using the signals

ODT1,SDCKE1, ZQ1 and CS1?

I am a little bit confused because in the Reference Manual for the i.MX

6ULL processor on page 2218 I found this Note:

NOTE

This feature will not be supported for DDR3 since only a single

chip select is supported for DDR3

Can you explain this to me?

Best regards

Michael

Mit freundlichen Grüßen

i. A. Dipl.Ing.(FH) Michael Nübling

Hardwareentwicklung

S. Siedle & Söhne Telefon- und Telegrafenwerke OHG

Bregstraße 1, 78120 Furtwangen

Telefon: +49 7723 63-307

Von: "igorpadykov" <admin@community.nxp.com>

An: "Michael Nübling" <michael.nuebling@siedle.de>

Datum: 10.05.2018 01:25

Betreff: Re: - Re: How to connect DDR3L to i.MX6 ULL

NXP Community

Re: How to connect DDR3L to i.MX6 ULL

reply from igorpadykov in i.MX Community - View the full discussion

Hi Michael

please look at i.MX6ULL EVK design files

Schematics (1)

Design files, including hardware schematics, Gerbers, and OrCAD files.

MCIMX6ULL-EVK_DESIGNFILES

http://www.nxp.com/products/software-and-tools/software-development-tools/

i.mx-software-and-tools/evaluation-kit-for-the-i.mx-6ull-applications-proc

essor:MCIMX6ULL-EVK?tab=Design_Tools_Tab

Best regards

igor

0 Kudos