How to connect 3.5 inch RGB LCD with i.MX6 Quad by use of TTL pins???

cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect 3.5 inch RGB LCD with i.MX6 Quad by use of TTL pins???

1,890 Views
jaymind
Contributor IV

Hello All,

I have LCD 6 bits RGB, 39 pins and I want to connect it with i.Mx6 Q use of Wand Board Quad..

I want to interface LCD with processor, and my LCD is RGB type 6 bits, 39 pins.
Also suggest me that where could I connect LCD control pins i.e. HSYNC, VSYNC, RESETB etc. with processor ???

There are 4 expansion headers on Wand Board Q, apart of therm one of header has TTL pins from 0 to 23 which connected to processor internally and one header has some control pins i.e. DSS_VSYNC, DSS_HSYNC etc.... which connected to processor at DISP0_CLK, DISP0_HSYNC, DISP0_VSYNC etc..

so main thing is that could I use this all pins (on JP1 and JP2) for interface my 39 pins, 6 bits RGB LCD ????

So please give any one suggest me that which pins of processor are support the RGB LCD connections and would there any driver or any type of converter needed for it to connect RGB LCD with processor by use of TTL pins (DISP0_DAT0 to DISP0_DAT23 and control pins) ????:smileyconfused:

Thanks in advance

Regards

Jaymin D

Labels (1)
Tags (3)
0 Kudos
1 Reply

113 Views
Yuri
NXP TechSupport
NXP TechSupport

  Please use i.MX6 Datasheet(s) to define typical IPU display output formats
and signals-to-pin mapping. For example please take a look at section 4.11.10.4
(IPU Display Interface Signal Mapping) of IMX6DQCEC (Rev. 3, 02/2014)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

    The i.MX6 LCD display signals are powered via NVCC_LCD, therefore voltage levels
of  display signals itself and the i.MX6 ones should match each other.

Have a great day,

Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos