How to confirm whether i.MX6SDL ERR007110 or ERR007220 occur.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to confirm whether i.MX6SDL ERR007110 or ERR007220 occur.

ソリューションへジャンプ
607件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6SDL.

Actually, their custom board does not boot from NAND only occasionally, and we doubt ERR007117 and ERR007220.

So we want to confirm whether this boot issue is cause by ERR007117 or ERR007220

Could you let me know how to confirm it?

Best Regards,

Satoshi Shimoda

ラベル(2)
0 件の賞賛
1 解決策
497件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

for ERR007117 one can attach jtag and output ENFC_CLK_ROOT

on CLKO pad using register CCM_CCOSR and check signal by oscilloscope.

For ERR007220 oen can add additional FCB records using

sect.8.5.2.2 "NAND Flash Boot Flow and Boot Control Blocks (BCB)"  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
498件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

for ERR007117 one can attach jtag and output ENFC_CLK_ROOT

on CLKO pad using register CCM_CCOSR and check signal by oscilloscope.

For ERR007220 oen can add additional FCB records using

sect.8.5.2.2 "NAND Flash Boot Flow and Boot Control Blocks (BCB)"  IMX6SDLRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛