How to configure the EIM of i.MX6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure the EIM of i.MX6?

4,807 Views
wanglee
Contributor III

    How to configure the EIM of i.MX6? Does anyone  have a Linux driver for communicating with a FPGA via the EIM port?  Multiplexed Addres/Data mode 16-bit.

Tags (1)
0 Kudos
5 Replies

3,082 Views
art
NXP Employee
NXP Employee

Currently, only parallel NOR Flash memory is supported on the EIM interface in the i.MX6 series Linux BSP. Please refer to the Chapter 42 of attached document for more information.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

3,082 Views
wanglee
Contributor III

HOW can I get  the i.MX6 series Linux BSP?

0 Kudos

3,082 Views
saurabh206
Senior Contributor III

Hi lee,

You can use Yocto for i.MX6 BSP.

Freescale Yocto Project main pae

Yocto Training - HOME

Thanks

Saurabh

0 Kudos

3,082 Views
wanglee
Contributor III

I find it

0 Kudos

3,082 Views
wanglee
Contributor III

Where is the attached document?

0 Kudos