How to configure ssi1_clk and clko_clk when used as i2s master sclk and mclk?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure ssi1_clk and clko_clk when used as i2s master sclk and mclk?

2,256 Views
fdact
Contributor I

Dear Sir or Madam,

                The default code I find ssi1_clk parent is pll3_pfd_508M and clko_clk parent is pll2_528_bus_main_clk that kernel version is 3.0.35.  In order to meet the requirements of master I2S , do I need to modify the clock parent?

                 I don't really understand the difference between the clock, such pll3_pfd_508M and pll2_528_bus_main_clk. Apart from the frequency and frequency of different multiples, what is the difference?

                 Now I set the parent clk for ssi1_clk and clko_clk to pll4, but I find I can't modify clko_clk and ssi1_clk less than 24mhz no matter how to change pll4 clock. 

                  Do you have any known ways to achieve this?

Thanks.

               

0 Kudos
Reply
4 Replies

1,887 Views
igorpadykov
NXP Employee
NXP Employee

Hi ferdinand

for ssi clock gneration one can look at attached document

Chapter 32 Configuring the SSI Driver.

Typical ssi clock values are given in Table 61-7. SSI Bit Clock and Frame Rate

i.MX6DQ RM http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,887 Views
fdact
Contributor I

Hi,

   Thanks for your reply .

    I have to configure the table according to this form. My problem is I can't modify ssi clock value less than 24MHZ, That form we can see the ssi clock can set 11.2896MHZ. So I try to modify ssi1_clk parent clk but also can't work.

Thanks.

0 Kudos
Reply

1,887 Views
igorpadykov
NXP Employee
NXP Employee

Table 61-7 shows typical values used with this processor,

and seems not all values can be obtained with default configuration.

0 Kudos
Reply

1,887 Views
fdact
Contributor I

Hi,

    "seems not all values can be obtained with default configuration" 。 But any value in a table can't be achieved. I already said clk can't less than 24MHZ, than means is no matter how calculate the pll and ssi clock the ssi clk always is 24MHZ.

Thanks.

0 Kudos
Reply