How to configure IMX6Q EIM Burst Synchronous to one BCLK one data?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure IMX6Q EIM Burst Synchronous to one BCLK one data?

2,762 Views
navyliang
Contributor I

Hello all,

      I use EIM to communicate with FPGA by Synchronous Mode, but have problems。

      I  according 《 i.MX 6Dual/6Quad Applications Processor Reference Manual》page 1046  22.8.9 Burst (Synchronous Mode) Write Memory Access Timing -BCD=1

pastedImage_9.png

I configure:read/write sync mode ,SWR=SRD=1, WFL=RFL=0,BL=2,PSZ=2

EIM_CS0GCR1=0X31135387

EIM_CSnGCR2=0

EIM_CSnWCR1= (16 << 24) | //WWSC=16

 EIM_CSnWCR2 =0

EIM_CSnRCR1=(16 << 24) | //RWSC=16

EIM_CSnRCR2=0

EIM_WCR=0

EIM_WIAR not configure
EIM_EAR not configure

in driver write:

   u32 buf_test[100] = {0x5001,0x5002,0x5003......}

   __raw_writew(buf_test, EIM_CS0_baseAddr);

But EIM  bus' data(sram_data) not  increase:

pastedImage_8.png

so, how i configure eim , when EIM_WAIT valid, one EIM_BCLK write or read one EIM_DATA?

I have been debugging for a long time. please help me, thank you!!

Labels (2)
0 Kudos
Reply
3 Replies

1,941 Views
bipin7301
Contributor II

Hi @navyliang 

I was also trying to do similar kind of thing but in i.MX7.

Were you able to achieve what you were trying to do ?

Can you please share your understanding/coding details ?

Regards

Bipin Kumar

0 Kudos
Reply

1,941 Views
igorpadykov
NXP Employee
NXP Employee

Hi Navy

please check example on

Sample code to use i.MX6DQ EIM burst access. 

i.MX6 maximum EIM burst length and performance  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,941 Views
xinhuah
Contributor I

Hi igorpadykov

    I have the same problem with Navy,the example Sample code to use i.MX6DQ EIM burst access is for IMX53,do you have the sample code for I.MX6DQ?

Thanks.

0 Kudos
Reply