How to configure IMX6 for Half duplex Mode in 1G speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure IMX6 for Half duplex Mode in 1G speed

785 Views
ashokp
Contributor I

Hi All,

I am using IMX6 custom board with latest yocto BSP from freescale. I want to configure the IMX6 Gigabit Ethernet as Half duplex mode. The ethtool shows in 1G (1000baseT) supports only Full duplex.

  Supported link modes:   10baseT/Half 10baseT/Full
                            100baseT/Half 100baseT/Full
                            1000baseT/Full
    Supported pause frame use: Symmetric
    Supports auto-negotiation: Yes
    Advertised link modes:  10baseT/Half 10baseT/Full
                            100baseT/Half 100baseT/Full
                            1000baseT/Full

Please let me know is there any patches or configurations available to enable Half duplex support in 1G speed.

Thanks,

P.Ashok.

Labels (3)
Tags (2)
0 Kudos
1 Reply

543 Views
b36401
NXP Employee
NXP Employee

No. We have no such patch.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos