How to configure IMX6 As a PCIe Endpoint?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure IMX6 As a PCIe Endpoint?

Jump to solution
1,325 Views
elijahbrown
Contributor III

Hi, I'm trying to configure the IMX6Q as a PCIe endpoint.  It's hooked up to another board which is the root complex.  I'm using the Freescale bare metal SDK PCIe test as a starting point.  I'm calling pcie_init() with the parameter PCIE_DM_MODE_EP instead of PCIE_DM_MODE_RC.  At this point the link will not come up.  I have a JTAG debugger hooked up and it seems like the CPU get stuck in the wait_link_up() function - it gets inside there and then the debugger is no longer able to halt the core.  If I set breakpoints and single step through wait_link_up(), it goes through OK but the link never succeeds.  Any ideas?  Is there code anywhere for the bare metal SDK to configure the PCIe as an endpoint instead of a root complex? 

Labels (2)
0 Kudos
1 Solution
831 Views
elijahbrown
Contributor III

Thanks, Norbel suggested we enable the 100MHz SATA clock in the ethernet PLL and that seems to have fixed the issue.  Now I need to figure out how to configure registers via DBI, I will post another thread about that. 

View solution in original post

0 Kudos
2 Replies
831 Views
igorpadykov
NXP Employee
NXP Employee

HI Elijah

please look at

i.MX6Q PCIe EP/RC Validation System

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
832 Views
elijahbrown
Contributor III

Thanks, Norbel suggested we enable the 100MHz SATA clock in the ethernet PLL and that seems to have fixed the issue.  Now I need to figure out how to configure registers via DBI, I will post another thread about that. 

0 Kudos