How to configure DISP0 to use 20 bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure DISP0 to use 20 bits

ソリューションへジャンプ
1,841件の閲覧回数
tw_imx53_
Contributor II

Hi,

I have a setup with a custom board connected to the i.MX53 QSB. Disp0 outputs 0-19 are connected to a serializer which needs the video data on following form:

In 0-9: 10 bits Chroma data

In 10-19: 10 bits Luma data

Video is coming out of the serializer, but the colors are not correct. I have tried different IPU_PIX_FMT_, but I am not sure what to select in order for the DI to output word aligned chroma/luma. If anybody has experience with this and can point me in the right direction, please let me know.

Edit:

Table 60 in the i.MX53 data sheet (IMX53CEC) lists different signal mappings for the display port. Can anyone please explain how to select for instance 16-bit YCrCb or 20-bit YCrCb from a kernel parameter, structure or register? For instance, when connecting the HDMI card to the QSB, "RGB24" kernel parameter obviously sets correct 24-bit RGB color mapping according to Table 60. But when selecting for instance YUV444 (or any YUV combos) the color space is clearly changing, but how can I know/find out how the Y/V signals are mapped out on the physical pins and whether it is 8-bit BT.656, 16-bit or 20-bit? I can not find any clear reference to this either in docs or code.

Thanks,

Trond

ラベル(3)
0 件の賞賛
返信
1 解決策
1,599件の閲覧回数
tw_imx53_
Contributor II

Made a temporary fix to adapt to my current hardware by modifying ipu_disp.c:_ipu_init_dc_mappings(). Instead of 10+10 bits I now zeroed out the two lsb of UV and Y words and shifted the eight bits accordingly to match my 20-bit interface with the 16 generated by i.MX using UYVY format. Colors are correct and I am happy.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,600件の閲覧回数
tw_imx53_
Contributor II

Made a temporary fix to adapt to my current hardware by modifying ipu_disp.c:_ipu_init_dc_mappings(). Instead of 10+10 bits I now zeroed out the two lsb of UV and Y words and shifted the eight bits accordingly to match my 20-bit interface with the 16 generated by i.MX using UYVY format. Colors are correct and I am happy.

0 件の賞賛
返信