How to configure CKO2 in IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure CKO2 in IMX6

1,181 Views
saritamahajan
Contributor I

Hii,

I am currently working on IMX6 Dart Board , for some purpose i need to generate 38 MHz on CKO2 which is currently providing 24MHz . so from where i can configure it? and what changes need to be done? As I am just beginner  in IMX6 series development , So any detailed steps can be helpful,

Thanks in advance. 

0 Kudos
Reply
1 Reply

1,074 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sarita

one can check AN4952 i.MX 6 Audio Clock Configuration Options

https://www.nxp.com/docs/en/application-note/AN4952.pdf 

For usage clocks in linux :

Linux common clock framework
https://www.kernel.org/doc/Documentation/clk.txt

https://elinux.org/images/b/b8/Elc2013_Clement.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply