update timing data provided by vendor
display-timings {
timing {
clock-frequency = <63000000>;
hactive = <720>;
vactive = <1280>;
hfront-porch = <12>;
hsync-len = <12>;
hback-porch = <24>;
vfront-porch = <10>;
vsync-len = <20>;
vback-porch = <20>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <0>;
pixelclk-active = <0>;
};
};
Vendor said it's base on MIPI bit rate 540MHz. After we apply this timing config, we still can't see anything on panel. I want to modify the mipi dsi data rate and clock to meet vendor's requirement. How can I do it? Please help advise the details. I found
/* Possible valid PHY reference clock rates*/
static u32 phyref_rates[] = {
27000000,
25000000,
24000000,
};
in Nwl-dsi.c. Is it what I am looking for? also, in Fsl-imx8mq.dtsi, we have below
mipi_dsi_bridge: mipi_dsi_bridge@30A00000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "nwl,mipi-dsi";
reg = <0x0 0x30A00000 0x0 0x400>;
interrupts = <GIC_SPI 34 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_DSI_PHY_REF>,
<&clk IMX8MQ_CLK_DSI_AHB>,
<&clk IMX8MQ_CLK_DSI_IPG_DIV>,
<&clk IMX8MQ_VIDEO_PLL1>;
clock-names = "phy_ref", "rx_esc", "tx_esc", "video_pll";
assigned-clocks = <&clk IMX8MQ_CLK_DSI_AHB>;
assigned-clock-parents = <&clk IMX8MQ_SYS1_PLL_80M>;
assigned-clock-rates = <80000000>;
phys = <&mipi_dsi_phy>;
phy-names = "dphy";
no_clk_reset;
status = "disabled";
port@0 {
mipi_dsi_bridge_in: endpoint {
remote-endpoint = <&mipi_dsi_out>;
};
};
};
Or I should modify these clock config to meet mipi dsi data rate and clock I need? (540MHz). How can I map these clock definition to real valuse?
thanks
CS