How to compile kernel in iMX6 UL EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to compile kernel in iMX6 UL EVK

1,744件の閲覧回数
adityaprajapati
Contributor I

Hello sir,

i want to compile device drivers and build kernel modules in my iMX6 board but i am, unable to find the

***********source code for the 4.1.15-1.1.0+ga4d2a08's kernel module**********

and i would even request you if you can guide me the procedure for the compiling of device driver too Thanks for the help in Advance With Regards Aditya

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,263件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Aditya Prajapat,

You can build customized images for the i.MX6UL EVK Board using the Linux BSP Release (link below, please note that you may need to login to download this file).

https://www.nxp.com/webapp/Download?colCode=L4.1.15_1.1.0_LINUX_DOCS

Please follow the Yocto User’s Guide document contained in this bundle. Since Yocto is used as a means of distribution the source code is fetched on demand. You may, however, fetch the required sources for a given image by using the following command:

bitbake <image_or_recipe> -c fetchall

You may also build the image and the source code will be available on the work directory.

<BUILD_DIR>/tmp/work/<MACHINE>-poky-linux-gnueabi/linux-imx/<KERNEL_REV>/git

I hope this information helps!

Regards,

0 件の賞賛
返信