How to comfirm my pcie bus is working fine?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to comfirm my pcie bus is working fine?

1,093件の閲覧回数
mingmingyuan
Contributor III

Dear FSL:

board:samba SD board

system:linux 3.0

Can you tell me how to confirm my pcie bus is working fine?

thanks

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

933件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mingming

one can check dmesg or lspci

dmesg - Wikipedia, the free encyclopedia

lspci - Wikipedia, the free encyclopedia

or run simple SDK PCIe test

i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

933件の閲覧回数
mingmingyuan
Contributor III

dear sir:

Thanks for your help!

I didn't connect any pcie device to my board, my logs as below, this is means that my pcie is ready?

iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.

PCIE: imx_pcie_pltfm_probe start link up.

IMX PCIe port: link up.

PCI: bus0: Fast back to back transfers disabled

PCI: bus1: Fast back to back transfers disabled

pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff 64bit pref]

pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff 64bit pref] (PCI address [0x1000000-0x10fffff])

pci 0000:00:00.0: BAR 9: assigned [mem 0x01100000-0x011fffff pref]

pci 0000:00:00.0: BAR 6: assigned [mem 0x01200000-0x0120ffff pref]

pci 0000:00:00.0: PCI bridge to [bus 01-01]

pci 0000:00:00.0:   bridge window [io  disabled]

pci 0000:00:00.0:   bridge window [mem disabled]

pci 0000:00:00.0:   bridge window [mem 0x01100000-0x011fffff pref]

0 件の賞賛
返信