How to check if DNS client is implemented in Sabre sd i.MX6Q board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to check if DNS client is implemented in Sabre sd i.MX6Q board

917 次查看
divyardharan
Contributor III

Hi all,

How to check if DNS client is implemented in Sabre sd i.MX6Q board?.dig and apt-get command not found in tera term(console).Kindly help.

Thanks,

Divya

标签 (1)
0 项奖励
回复
3 回复数

773 次查看
Yuri
NXP Employee
NXP Employee

  Please use the (Ubuntu) file-system from the Web demo image. 

https://www.freescale.com/webapp/Download?colCode=L3.0.101_4.1.1_IM6QDLS_BUNDLE&appType=license&loca...

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_DEMO_IMAGE_BSP&appType=license&locat...

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_UBUNTU_RFS_BSP&appType=license&locat...

Summary Page :i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

773 次查看
saurabh206
Senior Contributor III

Hi

Divya

Which build are using?

You can try Yocto build, check networking recipe for DNS implementation.

Thanks

Saurabh

0 项奖励
回复

773 次查看
divyardharan
Contributor III

Hi Saurabh,

Thank you for the fast responds. The build am using is ltib. Dig,apt-get commands are not found in the tera term.How to install these linux commands in Board.

Thanks,

Divya

0 项奖励
回复