How to check if DNS client is implemented in Sabre sd i.MX6Q board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to check if DNS client is implemented in Sabre sd i.MX6Q board

917件の閲覧回数
divyardharan
Contributor III

Hi all,

How to check if DNS client is implemented in Sabre sd i.MX6Q board?.dig and apt-get command not found in tera term(console).Kindly help.

Thanks,

Divya

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

773件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please use the (Ubuntu) file-system from the Web demo image. 

https://www.freescale.com/webapp/Download?colCode=L3.0.101_4.1.1_IM6QDLS_BUNDLE&appType=license&loca...

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_DEMO_IMAGE_BSP&appType=license&locat...

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_UBUNTU_RFS_BSP&appType=license&locat...

Summary Page :i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

773件の閲覧回数
saurabh206
Senior Contributor III

Hi

Divya

Which build are using?

You can try Yocto build, check networking recipe for DNS implementation.

Thanks

Saurabh

0 件の賞賛
返信

773件の閲覧回数
divyardharan
Contributor III

Hi Saurabh,

Thank you for the fast responds. The build am using is ltib. Dig,apt-get commands are not found in the tera term.How to install these linux commands in Board.

Thanks,

Divya

0 件の賞賛
返信