How to check PTM trace from the ETB without JTAG or Adaptor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to check PTM trace from the ETB without JTAG or Adaptor?

479 Views
pung2516
Contributor I

Hello People.

I am using I.MX6 solox Board.

Im trying to stack up my 'PTM trace' to the 'ETB' which is inside of the imx6sx board by setting the internal Register.

I don wanna use JTAG or other external adaptor or sth, Just wanna use the ETB in the imx6 solox board to pile up all of my PTM traces. 

Are there any specific settings for that?

Thx for your Help.

G1 Chang.

Labels (1)
0 Kudos
1 Reply

391 Views
igorpadykov
NXP Employee
NXP Employee

Hi G1 Chang

one can check arm documentation and post question on arm forum,

as it is not specific for i.mx

ARM Information Center 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos