How to change to ldo bypass mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change to ldo bypass mode?

Jump to solution
2,595 Views
kris_fei
Contributor III

Platform: IMX6DL
OS: Android 4.4
Kernel branch: 3.0.35

The temperature of our board is too high, i want to change to ldo bypass mode to low its temperature, 

how to configure it by software?

Labels (1)
1 Solution
2,293 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please refer to attached Release Notes

Table 6. Kernel Boot Parameters, parameter "ldo_active".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,294 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please refer to attached Release Notes

Table 6. Kernel Boot Parameters, parameter "ldo_active".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,293 Views
kris_fei
Contributor III

thanks, found it ~

0 Kudos
Reply