How to change the target core in an existing i.MX RT1170 project in windows

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to change the target core in an existing i.MX RT1170 project in windows

跳至解决方案
3,307 次查看
Shawn_
Contributor I

Hello everyone,

I am learning the demo of keyword spotting recently. I would like to ask, can I directly change the target core in an existing project? For example, the Demo of keyword spotting runs on CM7. Do I need to create a new project running on CM4 in MCUXpressoIDE, and then port the relevant code? Or is there any easier way?

Thanks and regards

标签 (2)
0 项奖励
回复
1 解答
3,294 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello!
Hope you are well.

Unfortunately, you need to port your code to a CM4 project to run it in CM4 core.
This post can be used as reference to create a multicore project: https://community.nxp.com/t5/i-MX-Processors/How-to-create-multi-core-project-with-MCUXpresso-IDE-fo...
Or you can start from an existing CM4 project and move your code to that project.


If you have more questions do not hesitate to ask me.
Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,295 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello!
Hope you are well.

Unfortunately, you need to port your code to a CM4 project to run it in CM4 core.
This post can be used as reference to create a multicore project: https://community.nxp.com/t5/i-MX-Processors/How-to-create-multi-core-project-with-MCUXpresso-IDE-fo...
Or you can start from an existing CM4 project and move your code to that project.


If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 项奖励
回复
3,269 次查看
Shawn_
Contributor I

Hi Omar,

Thanks for your answer, I still have a question about RT1170 core. Can I only use CM4 Core? I mean, can I boot the CM4 Core directly instead of booting the CM7 first, then wake up CM4 through CM7?

Thanks and Regards!

0 项奖励
回复
3,260 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, you can boot from the CM4 core. You can refer to chapter 2.2 from this application note: https://www.nxp.com/docs/en/application-note/AN13264.pdf

As NXP official SDK package only supports CM7 as main core (boot core), the enablement for this case is limited. Do not switch to CM4 as main core if it is not a must in your application.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 项奖励
回复