How to change the display Orientation in Android 10 hdmi port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to change the display Orientation in Android 10 hdmi port

399 次查看
subash_p
Contributor III

Hi,

I am working on an i.MX8MP custom board with Android 10_2.3.0. I am trying to change the display orientation from landscape to portrait in my Android image, so I added the following changes in my .mk files.

diff --git a/imx8m/BoardConfigCommon.mk b/imx8m/BoardConfigCommon.mk
index 92197b61..2b105592 100644
--- a/imx8m/BoardConfigCommon.mk
+++ b/imx8m/BoardConfigCommon.mk
@@ -10,7 +10,10 @@ HAVE_FSL_IMX_IPU \
PREBUILT_FSL_IMX_GPU \
BOARD_SOC_TYPE \
PRODUCT_MANUFACTURER \
-BOARD_VPU_ONLY
+BOARD_VPU_ONLY \
+SF_PRIMARY_DISPLAY_ORIENTATION
+
+SOONG_CONFIG_IMXPLUGIN_SF_PRIMARY_DISPLAY_ORIENTATION = 270

SOONG_CONFIG_IMXPLUGIN_BOARD_PLATFORM = imx8
SOONG_CONFIG_IMXPLUGIN_NUM_FRAMEBUFFER_SURFACE_BUFFERS = 3
diff --git a/imx8m/evk_8mm/BoardConfig.mk b/imx8m/evk_8mm/BoardConfig.mk
index ed30f771..cd8f4c89 100644
--- a/imx8m/evk_8mm/BoardConfig.mk
+++ b/imx8m/evk_8mm/BoardConfig.mk
@@ -117,6 +117,8 @@ TARGET_USES_MKE2FS := true
# define frame buffer count
NUM_FRAMEBUFFER_SURFACE_BUFFERS := 3

+SF_PRIMARY_DISPLAY_ORIENTATION := 270
+
ifeq ($(PRODUCT_IMX_DRM),true)
CMASIZE=736M
else


When I set SF_PRIMARY_DISPLAY_ORIENTATION := 270, the output appears in

landscape_view_android_10.jpeg

When I set SF_PRIMARY_DISPLAY_ORIENTATION := 180, the output appears in a

portrait_type_view_android_10.jpeg

,but not in the correct orientation. When i passed the 
$ settings put system user_rotation 3 command in android 15 means gives me the correct_portrait_view

correct_portrait_view.jpg

However, this command does not work on Android 11.

I will attach an image showing the orientation I am expecting in Android 10

correct_portrait_view.jpg


Thanks &Regards
Subash.P

 

标记 (4)
0 项奖励
回复
2 回复数

359 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

surfaceflinger rotation information will not pass to HWC in Android10, please try the attachment in HAL and use 'settings put system accelerometer_rotation 0/1' for test.

diff --git a/display/display/Composer.cpp b/display/display/Composer.cpp
old mode 100644
new mode 100755
index 8dba110..282c4f8
--- a/display/display/Composer.cpp
+++ b/display/display/Composer.cpp
@@ -350,11 +350,40 @@ int Composer::clearWormHole(LayerVector& layers)
 
 int Composer::composeLayer(Layer* layer, bool bypass)
 {
+	int transform;
     if (layer == NULL || mTarget == NULL) {
         ALOGE("composeLayer: invalid layer or target");
         return -EINVAL;
     }
 
+
+	/*
+		0 =>     4
+	   4  =>   3
+	   3  =>   7
+	   7  =>   0
+	*/
+	ALOGI("liutest1 composeLayer transform:0x%x\n",layer->transform);
+
+	switch (layer->transform)
+	{
+	case 0:
+		transform = 4;
+		break;
+	case 4:
+		transform = 3;
+		break;
+	case 3:
+		transform = 7;
+		break;
+	case 7:
+		transform = 0;
+		break;
+
+	default:
+		ALOGI("liutest1 invalid transform:0x%x\n",layer->transform);
+	}
+
     if (bypass && layer->isSolidColor()) {
         ALOGV("composeLayer dim layer bypassed");
         return 0;
@@ -392,7 +421,7 @@ int Composer::composeLayer(Layer* layer, bool bypass)
             continue;
         }
 
-        setClipping(srect, drect, clip, layer->transform);
+        setClipping(srect, drect, clip, /*layer->transform*/transform);
         ALOGV("index:%d, i:%d sourceCrop(l:%d,t:%d,r:%d,b:%d), "
              "visible(l:%d,t:%d,r:%d,b:%d), "
              "display(l:%d,t:%d,r:%d,b:%d)", layer->index, (int)i,
@@ -403,8 +432,9 @@ int Composer::composeLayer(Layer* layer, bool bypass)
             ALOGV("zorder:0x%x, layer phys:0x%" PRIx64,
                 layer->zorder, layer->handle->phys);
         }
-        ALOGV("transform:0x%x, blend:0x%x, alpha:0x%x",
-                layer->transform, layer->blendMode, layer->planeAlpha);
+        /*ALOGV*/ALOGI("liutest1 transform:0x%x:0x%x, blend:0x%x, alpha:0x%x",
+                layer->transform,transform, layer->blendMode, layer->planeAlpha);
+
 
         setG2dSurface(dSurfaceX, mTarget, drect);
 
@@ -422,7 +452,7 @@ int Composer::composeLayer(Layer* layer, bool bypass)
             return -EINVAL;
         }
 
-        convertRotation(layer->transform, sSurface, dSurface);
+        convertRotation(/*layer->transform*/transform, sSurface, dSurface);
         if (!bypass) {
             convertBlending(layer->blendMode, sSurface, dSurface);
         }



Best Regards,
Zhiming

0 项奖励
回复

346 次查看
subash_p
Contributor III

Hi @Zhiming_Liu 

After applying your patch, I can see some changes on my screen, but the resolution is not good. Also, when I connect a mouse, it works in the way of landscape navigation, not in portrait navigation. 

And also, the navigation bar is not visible.

a6a427ba-b133-4e1c-9cc8-b7fe694ef852.jpg


Best Regards,
Subash P.

标记 (4)
0 项奖励
回复