How to change the device name when plugin the usb with MTP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change the device name when plugin the usb with MTP mode

1,317件の閲覧回数
wangvictor
Contributor III

Hi I'm using i.MX6 sabresd with Android 6.0.

Now I'm facing the problem of changing the device name when plugin the usb.

This is the situation here.

When I choose this mode (Picture one) then PC will show the device name on the right bottom(Picture two) and the window will show up automatically (Picture three).

Picture one:

789.jpg

Picture two:

456.jpg

Picture three:

123.png

And I want to change all the device name M700DM8 to E500.

But I do not know how to do it.

Any advice?

Thanks in Advanced!

ラベル(4)
0 件の賞賛
返信
1 返信

1,213件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

I do not know if you are still having an issue.

But I just get notified that we cannot help you with your problem. Since we can be on legal issues for changing the USB name. I apologize for the inconvenience.

Best Regards,

Diego.

0 件の賞賛
返信