How to change the default PAD control values from U-boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change the default PAD control values from U-boot?

1,185 Views
hrushinale
Contributor III

Hello Community,

I am working on iMX6 solo based custom board.I am setting some PAD control values in my U-boot code but that values are not reflecting after U-boot boots up. So, I want to change the PAD control values after U-boot boot up , say suppose I want to set 0x1b0b0 to UART control PADS. How can I do that using u-boot coomand?

I know I have to use the mw command , but when I tried mw 20e0330 1b0b0 and then I tried reading at that address using md 20e0330 it didn't change the values to 1b0b0.

Kindly help me to solve this issue.

Best Regards,

Hrushi

Labels (1)
0 Kudos
Reply
1 Reply

1,047 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hrushi

could you try with mw.l and use nxp uboot 2016.03 :
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2016.03_4.1.15_2.0.0_ga

Also as IOMUX Control (IOMUXC) registers are valid DCD address, one can set its value

in dcd header.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply