How to change serial clock frequency in QSPI configuration parameters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change serial clock frequency in QSPI configuration parameters

ソリューションへジャンプ
2,519件の閲覧回数
takashi_kojima
Contributor I

Hello, Community.

Is there a way to change the serial clock frequency in the QSPI configuration parameters after system startup?

I want to set the serial clock frequency in the QSPI configuration parameter to 55MHz, and change it to 99MHz after the system boots.

I searched all QuadSPIx_xxx registers, but could not find any setting items for the serial clock frequency.

How do I change the serial clock frequency?

Best Regards,

Takashi Kojima

ラベル(1)
0 件の賞賛
返信
1 解決策
2,398件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

qspi clock generation is described in Figure 10-16. Flash Clock Diagram,

where ser_clk_4x is the serial clock root from CCM.

i.MX 7Dual Applications Processor Reference Manual

So it can be changed using CCM Table 5-11. Clock Root Table (QSPI_CLK_ROOT),

During boot with Table 6-50. QuadSPI configuration parameters, parameter "Serial Clock
Frequency".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,398件の閲覧回数
takashi_kojima
Contributor I

Hi, igor,
Thank you for your reply!

I understand that you can change serial clock frequency using Clock Root Table (QSPI_CLK_ROOT).

Best regards,
Takashi Kojima

0 件の賞賛
返信
2,399件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

qspi clock generation is described in Figure 10-16. Flash Clock Diagram,

where ser_clk_4x is the serial clock root from CCM.

i.MX 7Dual Applications Processor Reference Manual

So it can be changed using CCM Table 5-11. Clock Root Table (QSPI_CLK_ROOT),

During boot with Table 6-50. QuadSPI configuration parameters, parameter "Serial Clock
Frequency".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信