How to change otg gadget endpoints of communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change otg gadget endpoints of communication

1,192件の閲覧回数
linhaiboyy
Contributor II

Hi, 

   I am working on mx6q, mx6q as otg gadget device. I can use endpoints one communication with pc. But I can not use other  endpoints  communication with pc. How can i configure other endpoints ?

ラベル(1)
0 件の賞賛
返信
1 返信

1,104件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

usb driver handles endpoints automatically. Di you mean use several classes in one driver like

pic - One USB device with multiple device types? - Electrical Engineering Stack Exchange 

In general this is possible however custom driver should be implemented,

current usb driver supported features are described in attached Linux Manual Chapter 39
CHIPIDEA USB Driver.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信