How to change operation (/syatem/bin/)permission on imx6sl-evk board for marshmallow 6.0.1.2.0.0 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change operation (/syatem/bin/)permission on imx6sl-evk board for marshmallow 6.0.1.2.0.0 ?

2,677 Views
vinothpenati
Contributor I

Hi All,

     Last few days I am working in marshmallow bring on imx6sl-evk board.

     We were not able to access anything in /system/bin/ folder It showing Operation not permitted .

    

     Debug Logs ::

U-Boot 2015.04-14490-g596b7a8 (Aug 23 2016 - 15:48:28)

CPU:   Freescale i.MX6SL rev1.2 at 396 MHz

CPU:   Temperature 53 C

Reset cause: POR

Board: MX6SLEVK

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

In:    serial

Out:   serial

Err:   serial

Detecting VOL_DOWN+POWER key for recovery(0:0) ...

check_and_clean: reg 0, flag_set 0

Fastboot: Normal

flash target is MMC:1

Net:   FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

boota mmc1

kernel   @ 82808000 (8722408)

ramdisk  @ 83800000 (1028285)

fdt      @ 83700000 (36758)

## Booting Android Image at 0x80800000 ...

Kernel load addr 0x82808000 size 8518 KiB

Kernel command line: console=ttymxc0,115200 init=/init androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale

## Flattened Device Tree blob at 83700000

   Booting using the fdt blob at 0x83700000

   Loading Kernel Image ... OK

   Using Device Tree in place at 83700000, end 8370bf95

switch to ldo_bypass mode!

Starting kernel ...

Booting Linux on physical CPU 0x0

Initializing cgroup subsys cpu

Initializing cgroup subsys cpuacct

Linux version 4.1.15-226048-g082e62a (root@test) (gcc version 4.9.x-google 20140827 (prerelease) (GCC) ) #3 SMP PREEMPT Thu Aug 18 15:25:39 IST 2016

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine model: Freescale i.MX6 SoloLite EVK Board

Reserved memory: created CMA memory pool at 0x9a000000, size 320 MiB

Reserved memory: initialized node linux,cma, compatible id shared-dma-pool

Memory policy: Data cache writealloc

PERCPU: Embedded 13 pages/cpu @eef2d000 s22144 r8192 d22912 u53248

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260368

Kernel command line: console=ttymxc0,115200 init=/init androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale androidboot.serialno=051671d4dbc84cc3

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 690976K/1047552K available (11566K kernel code, 978K rwdata, 3688K rodata, 1024K init, 653K bss, 28896K reserved, 327680K cma-reserved, 269312K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)

    vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)

    lowmem  : 0xc0000000 - 0xef800000   ( 760 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .text : 0xc0008000 - 0xc0fe59fc   (16247 kB)

      .init : 0xc1000000 - 0xc1100000   (1024 kB)

      .data : 0xc1100000 - 0xc11f4890   ( 979 kB)

       .bss : 0xc11f4890 - 0xc1297f64   ( 654 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Preemptible hierarchical RCU implementation.

        Additional per-CPU info printed with stalls.

        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.

RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1

NR_IRQS:16 nr_irqs:16 16

L2C-310 erratum 769419 enabled

L2C-310 enabling early BRESP for Cortex-A9

L2C-310 full line of zeros enabled for Cortex-A9

L2C-310 ID prefetch enabled, offset 16 lines

L2C-310 dynamic clock gating enabled, standby mode enabled

L2C-310 cache controller enabled, 16 ways, 256 kB

L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76030001

mxc_clocksource_init 24000000

Switching to timer-based delay loop, resolution 41ns

sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns

clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)

pid_max: default: 32768 minimum: 301

Security Framework initialized

SELinux:  Initializing.

AppArmor: AppArmor disabled by boot time parameter

Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)

Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)

Initializing cgroup subsys freezer

Initializing cgroup subsys debug

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x80100000 - 0x80100058

Brought up 1 CPUs

SMP: Total of 1 processors activated (48.00 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

device-tree: Duplicate name in lcdif@020f8000, renamed to "display#1"

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns

pinctrl core: initialized pinctrl subsystem

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor ladder

cpuidle: using governor menu

anatop_regulator 20c8000.anatop:regulator-vddcore@140: Failed to read a valid default voltage selector.

anatop_regulator: probe of 20c8000.anatop:regulator-vddcore@140 failed with error -22

anatop_regulator 20c8000.anatop:regulator-vddsoc@140: Failed to read a valid default voltage selector.

anatop_regulator: probe of 20c8000.anatop:regulator-vddsoc@140 failed with error -22

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

VDSO is not a valid ELF object!

imx6sl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator

0-0048 supply SENSOR not found, using dummy regulator

i2c i2c-0: Max17135 PMIC not found!

i2c i2c-0: IMX I2C adapter registered

i2c i2c-0: can't use DMA

i2c i2c-1: IMX I2C adapter registered

i2c i2c-1: can't use DMA

i2c i2c-2: IMX I2C adapter registered

i2c i2c-2: can't use DMA

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.20

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

Switched to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 3, 32768 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 1008K (c3800000 - c38fc000)

CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]

hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available

imx rpmsg driver is registered.

Bus freq driver module loaded

console [pstore-1] enabled

pstore: Registered ramoops as persistent store backend

ramoops: attached 0x100000@0xbbf00000, ecc: 0/0

mxc_ramoops device success loaded

futex hash table entries: 256 (order: 2, 16384 bytes)

audit: initializing netlink subsys (disabled)

audit: type=2000 audit(0.580:1): initialized

VFS: Disk quotas dquot_6.6.0

VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

ntfs: driver 2.1.32 [Flags: R/W DEBUG].

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

fuse init (API version 7.23)

bounce: pool size: 64 pages

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

pwm-backlight supply power not found, using dummy regulator

MIPI DSI driver module loaded

MIPI DSI driver module loaded

sii902x 1-0039: Sii902x: cound not find device

mxsfb 20f8000.lcdif: failed to find mxc display driver

Console: switching to colour frame buffer device 100x30

mxsfb 20f8000.lcdif: initialized

imx-sdma 20ec000.sdma: no event needs to be remapped

imx-sdma 20ec000.sdma: loaded firmware 3.3

imx-sdma 20ec000.sdma: initialized

pfuze100-regulator 0-0008: Full layer: 1, Metal layer: 1

pfuze100-regulator 0-0008: FAB: 0, FIN: 0

pfuze100-regulator 0-0008: pfuze100 found.

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 21, base_baud = 5000000) is a IMX

console [ttymxc0] enabled

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

zram: Created 1 device(s)

m25p80 spi0.0: m25p32 (4096 Kbytes)

spi_imx 2008000.ecspi: probed

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

CAN device driver interface

2188000.ethernet supply phy not found, using dummy regulator

libphy: fec_enet_mii_bus: probed

PPP generic driver version 2.4.2

PPP BSD Compression module registered

PPP Deflate Compression module registered

PPP MPPE Compression module registered

NET: Registered protocol family 24

pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver

usbcore: registered new interface driver pegasus

usbcore: registered new interface driver rtl8150

usbcore: registered new interface driver r8152

usbcore: registered new interface driver asix

usbcore: registered new interface driver ax88179_178a

usbcore: registered new interface driver cdc_ether

usbcore: registered new interface driver cdc_eem

usbcore: registered new interface driver net1080

usbcore: registered new interface driver cdc_subset

usbcore: registered new interface driver zaurus

usbcore: registered new interface driver cdc_ncm

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-mxc: Freescale On-Chip EHCI Host driver

usbcore: registered new interface driver cdc_acm

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

usbcore: registered new interface driver usbserial_generic

usbserial: USB Serial support registered for generic

usbcore: registered new interface driver ftdi_sio

usbserial: USB Serial support registered for FTDI USB Serial Device

usbcore: registered new interface driver option

usbserial: USB Serial support registered for GSM modem (1-port)

usbcore: registered new interface driver usb_ehset_test

usb_otg1_vbus: supplied by SWBST

ci_hdrc ci_hdrc.0: EHCI Host Controller

ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: EHCI Host Controller

usb usb1: Manufacturer: Linux 4.1.15-226048-g082e62a ehci_hcd

usb usb1: SerialNumber: ci_hdrc.0

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

usb_otg2_vbus: supplied by SWBST

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

usb usb2: New USB device found, idVendor=1d6b, idProduct=0002

usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb2: Product: EHCI Host Controller

usb usb2: Manufacturer: Linux 4.1.15-226048-g082e62a ehci_hcd

usb usb2: SerialNumber: ci_hdrc.1

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

input: 20b8000.kpp as /devices/soc0/soc/2000000.aips-bus/20b8000.kpp/input/input0

usbcore: registered new interface driver xpad

usbcore: registered new interface driver usb_acecad

usbcore: registered new interface driver aiptek

usbcore: registered new interface driver gtco

usbcore: registered new interface driver hanwang

usbcore: registered new interface driver kbtab

mma8450 0-001c: read chip ID 0xfffffffb is not equal to 0xc6!

mma8450: probe of 0-001c failed with error -22

snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0

i2c /dev entries driver

IR NEC protocol handler initialized

IR RC5(x/sz) protocol handler initialized

IR RC6 protocol handler initialized

IR JVC protocol handler initialized

IR Sony protocol handler initialized

IR SANYO protocol handler initialized

IR Sharp protocol handler initialized

IR MCE Keyboard/mouse protocol handler initialized

IR XMP protocol handler initialized

2-003c supply DOVDD not found, using dummy regulator

ov5640_read_reg:write reg error:reg=300a

camera ov5640 is not found

pxp-v4l2 pxp_v4l2_out: initialized

usbcore: registered new interface driver uvcvideo

USB Video Class driver (1.1.1)

imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)

device-mapper: uevent: version 1.0.3

device-mapper: ioctl: 4.31.0-ioctl (2015-3-12) initialised: dm-devel@redhat.com

usb 1-1: new high-speed USB device number 2 using ci_hdrc

Bluetooth: HCI UART driver ver 2.3

Bluetooth: HCI UART protocol H4 registered

Bluetooth: HCI UART protocol BCSP registered

Bluetooth: HCI UART protocol ATH3K registered

usbcore: registered new interface driver btusb

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified

sdhci-esdhc-imx 2190000.usdhc: could not get ultra high speed state, work on normal mode

sdhci-esdhc-imx 2190000.usdhc: Got WP GPIO

sdhci-esdhc-imx 2190000.usdhc: assigned as wifi host

sdhci-esdhc-imx 2190000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found

mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using DMA

/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified

sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO

sdhci-esdhc-imx 2194000.usdhc: Got WP GPIO

sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found

usb 1-1: New USB device found, idVendor=05e3, idProduct=0608

usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0

usb 1-1: Product: USB2.0 Hub

hub 1-1:1.0: USB hub found

hub 1-1:1.0: 4 ports detected

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using DMA

/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified

sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on normal mode

sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found

mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using DMA

galcore: clk_get gpu3d_clk failed, disable 3d!

Galcore version 5.0.11.41671

mmc1: new high speed SDHC card at address e624

mmcblk1: mmc1:e624 SS08G 7.40 GiB

mmcblk1: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

mmcblk1: p4 size 12653270 extends beyond EOD, truncated

usb 1-1.3: new high-speed USB device number 3 using ci_hdrc

usb 1-1.3: New USB device found, idVendor=1618, idProduct=9113

usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=6

usb 1-1.3: Product: Wireless USB Network Module

usb 1-1.3: Manufacturer: Redpine Signals, Inc.

usb 1-1.3: SerialNumber: 000000000001

hidraw: raw HID events driver (C) Jiri Kosina

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

ashmem: initialized

usbcore: registered new interface driver snd-usb-audio

wm8962 1-001a: customer id 0 revision D

input: WM8962 Beep Generator as /devices/soc0/soc/2100000.aips-bus/21a4000.i2c/i2c-1/1-001a/input/input1

imx-wm8962 sound: wm8962 <-> 202c000.ssi mapping ok

imx-spdif sound-spdif: snd-soc-dummy-dai <-> 2004000.spdif mapping ok

NET: Registered protocol family 26

u32 classifier

    Actions configured

Netfilter messages via NETLINK v0.30.

nf_conntrack version 0.5.0 (15932 buckets, 63728 max)

ctnetlink v0.93: registering with nfnetlink.

xt_time: kernel timezone is -0000

ip_tables: (C) 2000-2006 Netfilter Core Team

arp_tables: (C) 2002 David S. Miller

Initializing XFRM netlink socket

NET: Registered protocol family 10

mip6: Mobile IPv6

ip6_tables: (C) 2000-2006 Netfilter Core Team

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

can: broadcast manager protocol (rev 20120528 t)

can: netlink gateway (rev 20130117) max_hops=1

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)

dhd_module_init in

Power-up adapter 'DHD generic adapter'

wifi_platform_bus_enumerate device present 1

failed to power up DHD generic adapter, 3 retry left

wifi_platform_bus_enumerate device present 0

wifi_platform_bus_enumerate device present 1

failed to power up DHD generic adapter, 2 retry left

wifi_platform_bus_enumerate device present 0

wifi_platform_bus_enumerate device present 1

failed to power up DHD generic adapter, 1 retry left

wifi_platform_bus_enumerate device present 0

wifi_platform_bus_enumerate device present 1

failed to power up DHD generic adapter, 0 retry left

wifi_platform_bus_enumerate device present 0

failed to power up DHD generic adapter, max retry reached**

snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 04:11:00 UTC (15060)

SW4: disabling

wm8962-supply-4v2: disabling

wm8962-supply-3v15: disabling

wlreg_on: disabling

ALSA device list:

  #0: wm8962-audio

  #1: imx-spdif

Freeing unused kernel memory: 1024K (c1000000 - c1100000)

init: init started!

SELinux:  Android master kernel running Android M policy in compatibility mode.

SELinux:  Permission audit_read in class capability2 not defined in policy.

SELinux: the above unknown classes and permissions will be denied

audit: type=1403 audit(15060.600:2): policy loaded auid=4294967295 ses=4294967295

audit: type=1404 audit(15060.620:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295

init: (Initializing SELinux enforcing took 0.12s.)

init: init second stage started!

init: waitpid failed: No child processes

init: property_set("ro.zygote", "zygote32") failed

init: (Loading properties from /default.prop took 0.00s.)

init: (Parsing /init.environ.rc took 0.00s.)

init: (Parsing /init.usb.rc took 0.00s.)

init: /init.freescale.rc: 288: ignored duplicate definition of service 'wpa_supplicant'

init: (Parsing init.freescale.usb.rc took 0.00s.)

init: (Parsing /init.freescale.rc took 0.01s.)

init: (Parsing /init.usb.configfs.rc took 0.00s.)

init: (Parsing /init.zygote32.rc took 0.00s.)

init: (Parsing /init.trace.rc took 0.00s.)

init: (Parsing /init.rc took 0.04s.)

init: SELinux: Could not get canonical path /adb_keys restorecon: No such file or directory.

init: Starting service 'ueventd'...

audit: type=1400 audit(15060.770:4): avc:  denied  { mounton } for  pid=1 comm="init" path="/sys/kernel/debug" dev="debugfs" ino=1 scontext=u:r:init:s0 tcontext=u:object_r:debugfs:s0 tclass=dir permissive0

ueventd: ueventd started!

init: Waiting for /dev/.coldboot_done...

ueventd: Coldboot took 0.32s.

init: Waiting for /dev/.coldboot_done took 0.32s.

init: Failed to read from /dev/hw_random: No such device

init: write_file: Unable to open '/proc/sys/kernel/sched_compat_yield': No such file or directory

init: write_file: Unable to write to '/dev/cpuctl/cpu.shares': Invalid argument

init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory

Console: switching to colour dummy device 80x30

init: Failed to read from /dev/hw_random: No such device

fs_mgr: Enabling dm-verity for system (mode 0)

EXT4-fs (dm-0): mounted filesystem with ordered data mode. Opts: barrier=1

fs_mgr: __mount(source=/dev/block/dm-0,target=/system,type=ext4)=0

EXT4-fs (mmcblk1p4): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk1p4): recovery complete

EXT4-fs (mmcblk1p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic

fs_mgr: __mount(source=/dev/block/mmcblk1p4,target=/data,type=ext4)=0

EXT4-fs (mmcblk1p6): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk1p6): recovery complete

EXT4-fs (mmcblk1p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit

fs_mgr: __mount(source=/dev/block/mmcblk1p6,target=/cache,type=ext4)=0

EXT4-fs (mmcblk1p7): mounted filesystem with ordered data mode. Opts: (null)

fs_mgr: __mount(source=/dev/block/mmcblk1p7,target=/device,type=ext4)=0

file system registered

init: Starting service 'logd'...

zram0: detected capacity change from 0 to 314572800

audit: type=1400 audit(15063.000:5): avc:  denied  { read write } for  pid=115 comm="mkswap" name="zram0" dev="tmpfs" ino=8193 scontext=u:r:toolbox:s0 tcontext=u:object_r:block_device:s0 tclass=blk_file p0

Unable to find swap-space signature

fs_mgr: swapon failed for /dev/block/zram0

logd.auditd: start

init: (Loading properties from /system/build.prop took 0.01s.)

logd.klogd: 14222211042

init: (Loading properties from /vendor/build.prop took 0.00s.)

init: (Loading properties from /factory/factory.prop took 0.00s.)

init: Starting service 'vold'...

init: Not bootcharting.

init: Starting service 'exec 0 (/system/bin/tzdatacheck)'...

init: Service 'exec 0 (/system/bin/tzdatacheck)' (pid 122) exited with status 0

random: init urandom read with 107 bits of entropy available

init: Starting service 'logd-reinit'...

init: Starting service 'healthd'...

init: Starting service 'console'...

binder: 126:126 transaction failed 29189, size 0-0

init: Starting service 'lmkd'...

init: Starting service 'servicemanager'...

init: Starting service 'surfaceflinger'...

init: write_file: Unable to open '/sys/block/mmcblk0/queue/read_ahead_kb': No such file or directory

init: Service 'logd-reinit' (pid 125) exited with status 194

root@evk_6sl:/ # logd.daemon: reinit

init: property_set("ro.ril.wake_lock_timeout", "300") failed

init: Starting service 'netd'...

init: Starting service 'debuggerd'...

init: cannot find '/system/bin/debuggerd64', disabling 'debuggerd64'

init: Starting service 'drm'...

init: Starting service 'media'...

init: Starting service 'installd'...

type=1400 audit(15063.610:6): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'

init: Starting service 'keystore'...

init: Starting service 'ril-daemon'...

init: Starting service 'zygote'...

init: Starting service 'gatekeeperd'...

init: cannot find '/system/xbin/perfprofd', disabling 'perfprofd'

random: nonblocking pool is initialized

healthd: BatteryTemperaturePath not found

healthd: BatteryTechnologyPath not found

init: Starting service 'bootanim'...

type=1400 audit(15063.630:7): avc: denied { dac_override } for pid=127 comm="sh" capability=1 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15063.660:8): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

type=1400 audit(15063.700:9): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

type=1400 audit(15063.710:10): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

type=1400 audit(15063.710:11): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

type=1400 audit(15063.710:12): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

type=1400 audit(15063.710:13): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

type=1400 audit(15063.740:14): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

type=1400 audit(15063.760:15): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

type=1400 audit(15063.780:16): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

type=1400 audit(15063.800:17): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

type=1400 audit(15063.810:18): avc: denied { sys_module } for pid=1 comm="init" capability=16 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0

capability: warning: `main' uses 32-bit capabilities (legacy support in use)

zram: 428 (system_server) Attribute mem_used_total (and others) will be removed. See zram documentation.

usb 1-1.1: new low-speed USB device number 4 using ci_hdrc

usb 1-1.1: New USB device found, idVendor=0461, idProduct=4e22

usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=0

usb 1-1.1: Product: USB Optical Mouse

usb 1-1.1: Manufacturer: PixArt

input: PixArt USB Optical Mouse as /devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/usb1/1-1/1-1.1/1-1.1:1.0/0003:0461:4E22.0001/input/input3

hid-generic 0003:0461:4E22.0001: input,hidraw0: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-ci_hdrc.0-1.1/input0

lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:

lowmemorykiller: oom_adj 0 => oom_score_adj 0

lowmemorykiller: oom_adj 1 => oom_score_adj 58

lowmemorykiller: oom_adj 2 => oom_score_adj 117

lowmemorykiller: oom_adj 3 => oom_score_adj 176

lowmemorykiller: oom_adj 9 => oom_score_adj 529

lowmemorykiller: oom_adj 15 => oom_score_adj 1000

type=1400 audit(15090.000:19): avc: denied { execute } for pid=474 comm="WifiStateMachin" name="sh" dev="dm-0" ino=518 scontext=u:r:system_server:s0 tcontext=u:object_r:shell_exec:s0 tclass=file permissiv0

acc_open

acc_release

fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:00, irq=-1)

IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

init: Starting service 'wpa_supplicant'...

init: Service 'wpa_supplicant' (pid 742) exited with status 255

root@evk_6sl:/ # cdinit: Service 'bootanim' (pid 162) exited with status 0

binder: undelivered transaction 7905

binder: undelivered transaction 7570

binder: undelivered transaction 5809

sybinder: release 903:903 transaction 8801 out, still active

binder: 428:798 transaction failed 29189, size 4-0

binder: send failed reply for transaction 8801, target dead

root@evk_6sl:/ # cd system/bbinder: release 989:989 transaction 10020 out, still active

binder: 428:683 transaction failed 29189, size 4-0

binder: send failed reply for transaction 10020, target dead

root@evk_6sl:/ # cd system/bin/relbinder: release 1076:1076 transaction 10603 out, still active

binder: 428:532 transaction failed 29189, size 4-0

binder: send failed reply for transaction 10603, target dead

root@evk_6sl:/ # cd system/bin/release/binder: release 1115:1115 transaction 10958 out, still active

binder: 428:439 transaction failed 29189, size 4-0

binder: send failed reply for transaction 10958, target dead

root@evk_6sl:/system/bin/release # binder: release 1128:1128 transaction 11057 out, still active

binder: 428:798 transaction failed 29189, size 4-0

binder: send failed reply for transaction 11057, target dead

sh o

onebox_common_gpl.ko      onebox_insert.sh          onebox_wlan_gpl.ko  

onebox_gpl.ko             onebox_nongpl.ko          onebox_wlan_nongpl.ko

h onebox_insert.sh type=1400 audit(15113.470:20): avc: denied { execute } for pid=1179 comm="WifiStateMachin" name="sh" dev="dm-0" ino=518 scontext=u:r:system_server:s0 tcontext=u:object_r:shell_exec:s0 t0

type=1400 audit(15113.940:21): avc: denied { dac_override } for pid=1182 comm="sh" capability=1 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

insmod: failed to load onebox_common_gpl.ko: Operation not permitted

insmod: failed to load wlan.ko: Operation not permitted

insmod: failed to load wlan_wep.ko: Operation not permitted

insmod: failed to load wlan_tkip.ko: Operation not permitted

insmod: failed to load wlan_ccmp.ko: Operation not permitted

insmod: failed to load wlan_acl.ko: Operation not permitted

insmod: failed to load wlan_xauth.ko: Operation not permitted

insmod: failed to load wlan_scan_sta.ko: Operation not permitted

insmod: failed to load onebox_wlan_nongpl.ko: Operation not permitted

insmod: failed to load onebox_wlan_gpl.ko: Operation not permitted

insmod: onebox_bt_nongpl.ko: No such file or directory

insmod: onebox_bt_gpl.ko: No such file or directory

insmod: onebox_zigb_nongpl.ko: No such file or directory

insmod: onebox_zigb_gpl.ko: No such file or directory

type=1400 audit(15114.020:22): avc: denied { sys_module } for pid=1183 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15114.090:23): avc: denied { sys_module } for pid=1184 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

insmod: failed to load onebox_nongpl.ko: Operation not permitted

insmod: failed to load onebox_gpl.ko: Operation not permitted

1|root@evk_6sl:/system/bin/release # type=1400 audit(15114.140:24): avc: denied { sys_module } for pid=1185 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permis0

type=1400 audit(15114.230:25): avc: denied { sys_module } for pid=1186 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15114.320:26): avc: denied { sys_module } for pid=1192 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15114.430:27): avc: denied { sys_module } for pid=1200 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15114.480:28): avc: denied { sys_module } for pid=1201 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15114.510:29): avc: denied { sys_module } for pid=1203 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15114.540:30): avc: denied { sys_module } for pid=1204 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15114.560:31): avc: denied { sys_module } for pid=1205 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15114.680:32): avc: denied { dac_override } for pid=1210 comm="sh" capability=1 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15114.740:33): avc: denied { sys_module } for pid=1211 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

type=1400 audit(15114.790:34): avc: denied { sys_module } for pid=1212 comm="insmod" capability=16 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0

init: Starting service 'wpa_supplicant'...

     My driver permissions are ,

              

-rwxr-xr-x root shell   26720 2016-08-23 09:06 onebox_common_gpl.ko
-rwxr-xr-x root shell   20792 2016-08-23 09:06 onebox_gpl.ko
-rwxr-xr-x root shell     644 2016-08-23 09:06 onebox_insert.sh
-rwxr-xr-x root shell   71304 2016-08-23 09:06 onebox_nongpl.ko
-rwxr-xr-x root shell   42024 2016-08-23 09:06 onebox_wlan_gpl.ko
-rwxr-xr-x root shell  168172 2016-08-23 09:06 onebox_wlan_nongpl.ko

Permissions are in executable only but its giving Operation not permitted.

Any solution for this issue ?

Thanks.

Labels (1)
0 Kudos
3 Replies

1,100 Views
prathapsimhadri
Contributor I

Hi Vinoth,

Did you got UI on lcd ?

Thanks,

Prathap.

0 Kudos

1,100 Views
b36401
NXP Employee
NXP Employee

Probably console is running not as root.
Please check it with "whoami" command.
If not you can use "su" to run commands as root.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,100 Views
gary_bisson
Senior Contributor III

Hi,

Looking at the log, it looks like SELinux doesn't allow you to do that.

Please modify the bootargs provided by U-Boot to the kernel to have 'androidboot.selinux=disabled'.

Regards,

Gary

0 Kudos