Hello NXP,
I want to edit the development board peripheral hardware (like GPIO, USB, LED..) and rebuild image
But I am not an expert in this area
For example, if I want to change the LED state (like power LED or else LED) by edit driver
How to do step by step ?
Thanks
you can refer to the dts file
for led, pls find
leds {
compatible = "gpio-leds";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_gpio_led>;
status {
label = "status";
gpios = <&gpio3 16 GPIO_ACTIVE_HIGH>;
default-state = "on";
};
Thanks for your reply
I connect the link but it show "Invalid branch: lf-5.15.y"
So I search other link about "imx8mm-evk.dts"
but I notice that 5.15.52 version have no "leds" part , why?
https://elixir.bootlin.com/linux/v5.15.52/source/arch/arm64/boot/dts/freescale/imx8mm-evk.dts
In addition, I try to control the GPIO like below link
https://variwiki.com/index.php?title=MX8_GPIO
I can use libgpiod command line to set GPIO
but when I use "libgpiod C Application" or "libgpiod Python Application"
C code can't find "gpiod.h" (use gcc to compile)
Python can't find "libgpiod.so"
My repo image is "imx-5.15.52.2.1.0"
How can I solve this issue
Thanks
Pls check the dtsi file instead of dts file, I mean imx8mm-evk.dtsi,
did you get this error when you cross compile your c source code?
Thanks for your reply
About "libgpiod C Application" or "libgpiod Python Application"
I use directly gcc compile on NXP terminal, it can't find "gpiod.h" or "libgpiod.so"
And you say "did you get this error when you cross compile your c source code?"
It means I need to add recipe or bblayer and bitbake?
If it is like this, what's the GPIO recipe or bblayer?
Thanks
did your source code includes them? I find an example, you can refer it
Following section provides examples how to use in Libgpiod
Following example shows how to get the state of a GPIO pin:
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include "gpiod.h"
int main(int argc, char * argv[]) {
struct gpiod_chip *chip;
struct gpiod_line *line;
char *dev;
int gpio_line;
int i, req, value = 0;
if (argc != 3)
{
printf("Wrong parameters \n \
Usage:\n \
./gpio_read_example <gpio_dev> <line>\n \
Example:\n \
./gpio_read_example /dev/gpiochip4 9 \n"
);
return -1;
}
dev = strdup(argv[1]);
if(!dev)
{
printf("Wrong CharDev Name\n");
return -1;
}
if (argv[2])
{
gpio_line = atoi(strdup(argv[2]));
}
chip = gpiod_chip_open(dev);
if (!chip)
return -1;
line = gpiod_chip_get_line(chip, gpio_line);
if (!line) {
gpiod_chip_close(chip);
return -1;
}
req = gpiod_line_request_input(line, "button");
if (req < 0) {
gpiod_chip_close(chip);
return -1;
}
value = gpiod_line_get_value(line);
printf("GPIO value of %s on line %d is: %d\n", dev, gpio_line, value);
gpiod_chip_close(chip);
}
Cross-Compilation
aarch64-linux-gnu-gcc gpio_read_example.c -I<workspace>/libgpiod/libgpiod_install/include -L<workspace>/libgpiod/libgpiod_install/lib -lgpiod -o gpio_read_example
./gpio_toggle_example /dev/gpiochip4 9
Thanks for your reply
Now I can use libgpiod C to control GPIO state
I control "exp_io9 " (gpiochip5 line 11) hight/low change
And I want to use another way to achieve ,like edit dts file and add driver
let it can default "gpiochip5 line 11" hight/low change when I boot
How can I do it step by step (use dts file and driver)?
Thanks
you can refer to the dts file, which has gpio configuration, then config your own gpio, the detailed settings, pls refer to the reference manual, you also can refer to the document as below