How to change i.MX6 CPU frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change i.MX6 CPU frequency

4,811 Views
frankchenmh
Contributor III

Hi, I use i.MX6 Android KK4.4.2 BSP. I noticed the CPU run at 792MHz because I can see the following message when uboot boots up:

CPU: Freescale i.MX6 family TO1.5 at 792 MHz

Could anyone let me know how to change i.MX6 CPU frequency to 1GHz or 1.2GHz? Thanks!

Labels (5)
0 Kudos
Reply
2 Replies

3,412 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Frank,

Which i.mx6 processor are you using? Firstly, you need to confirm if it support 1.2Ghz work.

About how to change you can refer to the follow thread:

How can I change CPU frequency on i.MX6Q ? 

Change CPU frequency 

https://community.nxp.com/message/662973 

Hope this can help you. Any questions you can conact me.


Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,412 Views
frankchenmh
Contributor III

Hi Rita,

Thanks for you reply! I can now change CPU frequency to 1GHz based on your info. I will study if it can be changed to 1.2GHz.

We have some i.MX6Q chips which support 1.2GHz.

0 Kudos
Reply