Hi Jerry
some customers succeeded with patch, output on clko
diff --git a/arch/arm/mach-imx/clk-imx6q.c b/arch/arm/mach-imx/clk-imx6q.c
index f0d8000..a22dbb5
--- a/arch/arm/mach-imx/clk-imx6q.c
+++ b/arch/arm/mach-imx/clk-imx6q.c
@@ -543,11 +543,14 @@ static void __init imx6q_clocks_init(struct device_node *ccm_node)
}
/*
- * Let's initially set up CLKO with OSC24M, since this configuration
- * is widely used by imx6q board designs to clock audio codec.
+ * Pll4 -> ssi2 -> clko2 -> clko
*/
- imx_clk_set_parent(clk[IMX6QDL_CLK_CKO2_SEL], clk[IMX6QDL_CLK_OSC]);
imx_clk_set_parent(clk[IMX6QDL_CLK_CKO], clk[IMX6QDL_CLK_CKO2]);
+ imx_clk_set_parent(clk[IMX6QDL_CLK_SSI2_SEL], clk[IMX6QDL_CLK_PLL4_AUDIO_DIV]);
+ imx_clk_set_parent(clk[IMX6QDL_CLK_CKO2_SEL], clk[IMX6QDL_CLK_SSI2]);
+
+ imx_clk_set_rate(clk[IMX6QDL_CLK_PLL4_AUDIO_DIV], 196608000);
+ imx_clk_set_rate(clk[IMX6QDL_CLK_SSI2], 196608000/8);
/* Audio-related clocks configuration */
imx_clk_set_parent(clk[IMX6QDL_CLK_SPDIF_SEL], clk[IMX6QDL_CLK_PLL3_PFD3_454M]);
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jerry
some customers succeeded with patch, output on clko
diff --git a/arch/arm/mach-imx/clk-imx6q.c b/arch/arm/mach-imx/clk-imx6q.c
index f0d8000..a22dbb5
--- a/arch/arm/mach-imx/clk-imx6q.c
+++ b/arch/arm/mach-imx/clk-imx6q.c
@@ -543,11 +543,14 @@ static void __init imx6q_clocks_init(struct device_node *ccm_node)
}
/*
- * Let's initially set up CLKO with OSC24M, since this configuration
- * is widely used by imx6q board designs to clock audio codec.
+ * Pll4 -> ssi2 -> clko2 -> clko
*/
- imx_clk_set_parent(clk[IMX6QDL_CLK_CKO2_SEL], clk[IMX6QDL_CLK_OSC]);
imx_clk_set_parent(clk[IMX6QDL_CLK_CKO], clk[IMX6QDL_CLK_CKO2]);
+ imx_clk_set_parent(clk[IMX6QDL_CLK_SSI2_SEL], clk[IMX6QDL_CLK_PLL4_AUDIO_DIV]);
+ imx_clk_set_parent(clk[IMX6QDL_CLK_CKO2_SEL], clk[IMX6QDL_CLK_SSI2]);
+
+ imx_clk_set_rate(clk[IMX6QDL_CLK_PLL4_AUDIO_DIV], 196608000);
+ imx_clk_set_rate(clk[IMX6QDL_CLK_SSI2], 196608000/8);
/* Audio-related clocks configuration */
imx_clk_set_parent(clk[IMX6QDL_CLK_SPDIF_SEL], clk[IMX6QDL_CLK_PLL3_PFD3_454M]);
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
following previous question. i set sysclk manually, when i set sysclk to mclk( it equals to 512Fs) , it reports ""failed to handle the required sysclk". when I set sysclk to mclk/2 (it equals to 256Fs) , it reports "failed to set baudclk rate\n". Then i check the function fsl_ssi_set_bclk((), in which , two other clk are used , "ipg" and "baud" , these two clk are defined in dts as
ssi2:{
......
clocks = <&clks IMX6QDL_CLK_SSI2_IPG>,
<&clks IMX6QDL_CLK_SSI2>;
clock-names = "ipg", "baud";
....
}
i checked the clk_rate of ssi2_ipg, it is 66000000.
Is there anyone who has the experience of such case?
Thanks in advance.
Hi Igor,
Thanks for your quick answer . it works .
I have another question, I use SSI to connect to a CS4244(CS42888 like) codec, and need to use TDM mode . The CS4244 has 4 ADC and 4 DAC , and only work on 8 or 16 slots in TDM mode, so the SCLK should be 256xFs or 512xFs. I use the same ALSA config file as CS42888 to use device surround40 , which has 4 channels. But in fsl_ssi.c, if 4 channels used, the BCLK will be set to 4*32*Fs=128Fs, but codec can not work on this freq. The linux kernel version is 4.1.15.
Best Regards