Hello nxf63675,
Thank you for reply,
1.
I have referred reference manual and make changes accordingly but ddr frequency doesn't changes. I have referred below patch for the make changes in the kernel.
2.
Also I have check below nxp community thread.
https://community.nxp.com/t5/i-MX-Processors/Change-LPDDR4-operating-frequency/m-p/862861
In above thread
dram_core_clk --- 000010a0 1 1 800000000 "dram_core_clk=800" means DRAM Clock=1600 (DDRC PHY PLL multiplies the input
we have checked on board its also showing: ----------------------------------------------------------------------------------
dram_pll1_ref_sel 1 1 0 25000000 0 0 50000
dram_pll_out 2 2 0 800000000 0 0 50000
dram_core_clk 1 1 0 800000000 0 0 50000
dram_alt 0 0 0 250000000 0 0 50000
dram_alt_root 0 0 0 62500000 0 0 50000
dram_apb 1 1 0 160000000 0 0 50000
------------------------------------------------------------------------------------
but when we probe DDR frequency in DSO, its showing pick at 800 MHz only.