I have a problem with passing raw data from sensor.
Sensor sends 10bit packed data, I try to get 8bit MSB but I get probably 8bit LSB.
Also I get low framerate.
Attached kernel patches, and sample image.
Commands used in testing:
GST_DEBUG=3 gst-launch-1.0 -v v4l2src device=/dev/video3 ! "video/x-raw,width=1440,height=1088,format=GRAY8" ! videoconvert ! video/x-raw,format=I420 ! jpegenc ! queue ! rtpjpegpay ! udpsink host=192.168.1.164 port=18888 sync=false
GST_DEBUG=3 gst-launch-1.0 -v v4l2src device=/dev/video3 num-buffers=1 ! "video/x-raw,width=1440,height=1088,format=GRAY8" ! pngenc ! filesink location=a.png
Kernel dump with registers:
[ 1236.732055] Custom device pixelformat 0x30535641 'AVS Encoded Stream'
[ 1236.732086] Custom device pixelformat 0x58564944 'DIVX Encoded Stream'
[ 1236.732102] Custom device pixelformat 0x30305652 'RV Encoded Stream'
[ 1236.732110] Custom device pixelformat 0x30365056 'VP6 Encoded Stream'
[ 1236.732117] Custom device pixelformat 0x304b5053 'SPK Encoded Stream'
[ 1236.732138] Custom device pixelformat 0x43564548 'H265 HEVC Encoded Stream'
[ 1236.732147] Custom device pixelformat 0x4f474f4c 'Logo'
[ 1236.732260] Custom device pixelformat 0x3231544e '4:2:0 2 Planes Y/CbCr'
[ 1236.737350] mxc-jpeg 58400000.jpegdec: Descriptor for dec/enc: ffff000008e57000 0x96002000
[ 1236.737359] mxc-jpeg 58400000.jpegdec: Descriptor for config phase: ffff000008e58000 0x96003000
[ 1236.737365] mxc-jpeg 58400000.jpegdec: Configuration stream: ffff000008e59000 0x96004000
[ 1236.738114] mxc-jpeg 58450000.jpegenc: Descriptor for dec/enc: ffff000008e57000 0x96002000
[ 1236.738120] mxc-jpeg 58450000.jpegenc: Descriptor for config phase: ffff000008e58000 0x96003000
[ 1236.738126] mxc-jpeg 58450000.jpegenc: Configuration stream: ffff000008e59000 0x96004000
[ 1236.739424] mxc-isi 58140000.isi: mxc_isi_capture_open, ISI4
[ 1236.770964] mxc-isi 58140000.isi: mxc_isi_capture_release
[ 1236.776120] mxc-isi 58100000.isi: mxc_isi_m2m_open, ISI0
[ 1236.781384] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_out
[ 1236.781426] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_out
[ 1236.781455] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_out
[ 1236.781466] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_out
[ 1236.781494] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_out
[ 1236.781520] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_out
[ 1236.781619] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_cap
[ 1236.781648] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_cap
[ 1236.781675] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_cap
[ 1236.781702] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_cap
[ 1236.781728] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_cap
[ 1236.781739] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_cap
[ 1236.781769] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_cap
[ 1236.781780] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_cap
[ 1236.781807] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_cap
[ 1236.781832] mxc-isi 58100000.isi: mxc_isi_m2m_enum_fmt_vid_cap
[ 1236.782504] mxc-isi 58100000.isi: mxc_isi_m2m_release
[ 1236.802959] mxc-isi 58140000.isi: mxc_isi_capture_open, ISI4
[ 1236.835723] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835741] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835763] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835774] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835785] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835795] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835805] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835817] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835827] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835837] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835848] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835869] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835882] mxc-isi 58140000.isi: mxc_isi_cap_enum_fmt_mplane
[ 1236.835896] mxc-isi 58140000.isi: mxc_isi_cap_g_selection
[ 1236.836717] mxc-isi 58140000.isi: mxc_isi_cap_s_fmt_mplane, fmt=0x59455247
[ 1236.838605] mxc-isi 58140000.isi: cap_vb2_queue_setup, buf_n=2, size=1566720
[ 1236.843381] mxc-isi 58140000.isi: cap_vb2_buffer_prepare
[ 1236.843422] mxc-isi 58140000.isi: cap_vb2_buffer_prepare
[ 1236.843460] mxc-isi 58140000.isi: mxc_isi_cap_streamon
[ 1236.843484] mxc-mipi-csi2 58247000.csi: width=1440, height=1088, fmt.code=0x300f
[ 1236.848509] bypass csc
[ 1236.849568] input fmt RG10
[ 1236.850971] output fmt GREY
[ 1236.852491] mxc-isi 58140000.isi: mxc_isi_channel_set_scaling: no scale
[ 1236.852506] mxc-isi 58140000.isi: cap_vb2_start_streaming
[ 1236.855521] mxc-isi 58140000.isi: cap_vb2_start_streaming: num_plane=0 discard_size=1566720 discard_buffer=ffff000025181000
[ 1237.159955] mxc-isi 58140000.isi: ISI CHNLC register dump, isi4
[ 1237.159964] mxc-isi 58140000.isi: CHNL_CTRL 0x0h = 0xe0ff0003
[ 1237.159972] mxc-isi 58140000.isi: CHNL_IMG_CTRL 0x4h = 0x b000001
[ 1237.159979] mxc-isi 58140000.isi: CHNL_OUT_BUF_CTRL 0x8h = 0x 8000
[ 1237.159986] mxc-isi 58140000.isi: CHNL_IMG_CFG 0xCh = 0x 44005a0
[ 1237.159993] mxc-isi 58140000.isi: CHNL_IER 0x10h = 0x3dff0000
[ 1237.160000] mxc-isi 58140000.isi: CHNL_STS 0x14h = 0x 200
[ 1237.160007] mxc-isi 58140000.isi: CHNL_SCALE_FACTOR 0x18h = 0x10001000
[ 1237.160013] mxc-isi 58140000.isi: CHNL_SCALE_OFFSET 0x1Ch = 0x 0
[ 1237.160020] mxc-isi 58140000.isi: CHNL_CROP_ULC 0x20h = 0x 0
[ 1237.160026] mxc-isi 58140000.isi: CHNL_CROP_LRC 0x24h = 0x 0
[ 1237.160032] mxc-isi 58140000.isi: CHNL_CSC_COEFF0 0x28h = 0x 0
[ 1237.160038] mxc-isi 58140000.isi: CHNL_CSC_COEFF1 0x2Ch = 0x 0
[ 1237.160044] mxc-isi 58140000.isi: CHNL_CSC_COEFF2 0x30h = 0x 0
[ 1237.160051] mxc-isi 58140000.isi: CHNL_CSC_COEFF3 0x34h = 0x 0
[ 1237.160057] mxc-isi 58140000.isi: CHNL_CSC_COEFF4 0x38h = 0x 0
[ 1237.160063] mxc-isi 58140000.isi: CHNL_CSC_COEFF5 0x3Ch = 0x 0
[ 1237.160069] mxc-isi 58140000.isi: CHNL_ROI_0_ALPHA 0x40h = 0x 0
[ 1237.160076] mxc-isi 58140000.isi: CHNL_ROI_0_ULC 0x44h = 0x 0
[ 1237.160082] mxc-isi 58140000.isi: CHNL_ROI_0_LRC 0x48h = 0x 0
[ 1237.160088] mxc-isi 58140000.isi: CHNL_ROI_1_ALPHA 0x4Ch = 0x 0
[ 1237.160094] mxc-isi 58140000.isi: CHNL_ROI_1_ULC 0x50h = 0x 0
[ 1237.160101] mxc-isi 58140000.isi: CHNL_ROI_1_LRC 0x54h = 0x 0
[ 1237.160107] mxc-isi 58140000.isi: CHNL_ROI_2_ALPHA 0x58h = 0x 0
[ 1237.160114] mxc-isi 58140000.isi: CHNL_ROI_2_ULC 0x5Ch = 0x 0
[ 1237.160120] mxc-isi 58140000.isi: CHNL_ROI_2_LRC 0x60h = 0x 0
[ 1237.160126] mxc-isi 58140000.isi: CHNL_ROI_3_ALPHA 0x64h = 0x 0
[ 1237.160132] mxc-isi 58140000.isi: CHNL_ROI_3_ULC 0x68h = 0x 0
[ 1237.160139] mxc-isi 58140000.isi: CHNL_ROI_3_LRC 0x6Ch = 0x 0
[ 1237.160145] mxc-isi 58140000.isi: CHNL_OUT_BUF1_ADDR_Y 0x70h = 0xa6800000
[ 1237.160151] mxc-isi 58140000.isi: CHNL_OUT_BUF1_ADDR_U 0x74h = 0x 0
[ 1237.160158] mxc-isi 58140000.isi: CHNL_OUT_BUF1_ADDR_V 0x78h = 0x 0
[ 1237.160164] mxc-isi 58140000.isi: CHNL_OUT_BUF_PITCH 0x7Ch = 0x 5a0
[ 1237.160170] mxc-isi 58140000.isi: CHNL_IN_BUF_ADDR 0x80h = 0x 0
[ 1237.160176] mxc-isi 58140000.isi: CHNL_IN_BUF_PITCH 0x84h = 0x 0
[ 1237.160182] mxc-isi 58140000.isi: CHNL_MEM_RD_CTRL 0x88h = 0x 0
[ 1237.160189] mxc-isi 58140000.isi: CHNL_OUT_BUF2_ADDR_Y 0x8Ch = 0xa6400000
[ 1237.160195] mxc-isi 58140000.isi: CHNL_OUT_BUF2_ADDR_U 0x90h = 0x 0
[ 1237.160201] mxc-isi 58140000.isi: CHNL_OUT_BUF2_ADDR_V 0x94h = 0x 0
[ 1237.160213] mxc-md camera: begin graph walk at 'mxc_isi.4.capture'
[ 1237.160221] mxc-md camera: walk: pushing 'mxc_isi.4' on stack
[ 1237.160228] mxc-md camera: walk: skipping entity 'mxc_isi.4.capture' (already seen)
[ 1237.160235] mxc-md camera: walk: pushing 'mxc-mipi-csi2.1' on stack
[ 1237.160242] mxc-md camera: walk: skipping entity 'mxc_isi.4' (already seen)
[ 1237.160248] mxc-md camera: walk: pushing 'imx296 6-001a' on stack
[ 1237.160255] mxc-md camera: walk: skipping entity 'mxc-mipi-csi2.1' (already seen)
[ 1237.160261] mxc-md camera: walk: returning entity 'imx296 6-001a'
[ 1237.252430] mxc-md camera: walk: returning entity 'mxc-mipi-csi2.1'
[ 1237.252442] mxc-mipi-csi2 58247000.csi: mipi_csi2_s_stream: 1, csi2dev: 0x0
[ 1237.252490] mxc-mipi-csi2 58247000.csi: width=1440, height=1088, fmt.code=0x300f
[ 1237.252513] MIPI CSI2 HC register dump, mipi csi1
[ 1237.255957] MIPI CSI2 HC num of lanes 0x100 = 0x0
[ 1237.259710] MIPI CSI2 HC dis lanes 0x104 = 0xe
[ 1237.263489] MIPI CSI2 HC BIT ERR 0x108 = 0x0
[ 1237.267254] MIPI CSI2 HC IRQ STATUS 0x10C = 0x8
[ 1237.271094] MIPI CSI2 HC IRQ MASK 0x110 = 0x1ff
[ 1237.275033] MIPI CSI2 HC ULPS STATUS 0x114 = 0x0
[ 1237.278804] MIPI CSI2 HC DPHY ErrSotHS 0x118 = 0x0
[ 1237.282569] MIPI CSI2 HC DPHY ErrSotSync 0x11c = 0x0
[ 1237.286342] MIPI CSI2 HC DPHY ErrEsc 0x120 = 0x0
[ 1237.290101] MIPI CSI2 HC DPHY ErrSyncEsc 0x124 = 0x0
[ 1237.293873] MIPI CSI2 HC DPHY ErrControl 0x128 = 0x0
[ 1237.297632] MIPI CSI2 HC DISABLE_PAYLOAD 0x12C = 0x0
[ 1237.301405] MIPI CSI2 HC DISABLE_PAYLOAD 0x130 = 0x0
[ 1237.305167] MIPI CSI2 HC IGNORE_VC 0x180 = 0x0
[ 1237.308936] MIPI CSI2 HC VID_VC 0x184 = 0x0
[ 1237.312700] MIPI CSI2 HC FIFO_SEND_LEVEL 0x188 = 0x0
[ 1237.316468] MIPI CSI2 HC VID_VSYNC 0x18C = 0x0
[ 1237.320253] MIPI CSI2 HC VID_SYNC_FP 0x190 = 0x0
[ 1237.324026] MIPI CSI2 HC VID_HSYNC 0x194 = 0x0
[ 1237.327777] MIPI CSI2 HC VID_HSYNC_BP 0x198 = 0x0
[ 1237.332315] MIPI CSI2 CSR register dump
[ 1237.334847] MIPI CSI2 CSR PLM_CTRL 0x000 = 0x801
[ 1237.338784] MIPI CSI2 CSR PHY_CTRL 0x004 = 0x2000af
[ 1237.343703] MIPI CSI2 CSR PHY_Status 0x008 = 0x1
[ 1237.347468] MIPI CSI2 CSR PHY_Test_Status 0x010 = 0x0
[ 1237.351218] MIPI CSI2 CSR PHY_Test_Status 0x014 = 0x0
[ 1237.355726] MIPI CSI2 CSR PHY_Test_Status 0x018 = 0x0
[ 1237.359482] MIPI CSI2 CSR PHY_Test_Status 0x01C = 0x0
[ 1237.363238] MIPI CSI2 CSR PHY_Test_Status 0x020 = 0x0
[ 1237.366985] MIPI CSI2 CSR VC Interlaced 0x030 = 0x0
[ 1237.370733] MIPI CSI2 CSR Data Type Dis 0x038 = 0x0
[ 1237.374482] MIPI CSI2 CSR 420 1st type 0x040 = 0x0
[ 1237.378232] MIPI CSI2 CSR Ctr_Ck_Rst_Ctr 0x044 = 0x1
[ 1237.381984] MIPI CSI2 CSR Stream Fencing 0x048 = 0x0
[ 1237.385736] MIPI CSI2 CSR Stream Fencing 0x04C = 0x0
[ 1237.389489] mxc-md camera: walk: returning entity 'mxc_isi.4'
[ 1237.389492] mxc-md camera: walk: returning entity 'mxc_isi.4.capture'
[ 1237.389495] mxc-isi 58140000.isi: mxc_isi_pipeline_enable ,entity is no v4l2, mxc_isi.4.capture
[ 1237.389738] vb2_common_vm_open: ffff8008781c4d48, refcount: 2, vma: ffff843a4000-ffff84523000
[ 1237.389742] vb2_dc_mmap: mapped dma addr 0xa6400000 at 0xffff843a4000, size 1568768
[ 1238.347293] mxc-isi 58140000.isi: cap_vb2_buffer_prepare
[ 1238.351766] mxc-isi 58140000.isi: mxc_isi_cap_streamoff
[ 1238.351776] mxc-md camera: begin graph walk at 'mxc_isi.4.capture'
[ 1238.351782] mxc-md camera: walk: pushing 'mxc_isi.4' on stack
[ 1238.351787] mxc-md camera: walk: skipping entity 'mxc_isi.4.capture' (already seen)
[ 1238.351791] mxc-md camera: walk: pushing 'mxc-mipi-csi2.1' on stack
[ 1238.351795] mxc-md camera: walk: skipping entity 'mxc_isi.4' (already seen)
[ 1238.351800] mxc-md camera: walk: pushing 'imx296 6-001a' on stack
[ 1238.351804] mxc-md camera: walk: skipping entity 'mxc-mipi-csi2.1' (already seen)
[ 1238.351808] mxc-md camera: walk: returning entity 'imx296 6-001a'
[ 1238.392256] mxc-md camera: walk: returning entity 'mxc-mipi-csi2.1'
[ 1238.392268] mxc-mipi-csi2 58247000.csi: mipi_csi2_s_stream: 0, csi2dev: 0x0
[ 1238.392355] mxc-md camera: walk: returning entity 'mxc_isi.4'
[ 1238.392363] mxc-md camera: walk: returning entity 'mxc_isi.4.capture'
[ 1238.392371] mxc-isi 58140000.isi: mxc_isi_pipeline_enable ,entity is no v4l2, mxc_isi.4.capture
[ 1238.392382] mxc-isi 58140000.isi: cap_vb2_stop_streaming
[ 1238.393247] vb2_common_vm_close: ffff8008781c4d48, refcount: 3, vma: ffff843a4000-ffff84523000
[ 1238.396300] mxc-isi 58140000.isi: mxc_isi_capture_release
I'm afraid I cannot. It uses proprietary libraries, and not optimalized enough (720p <15fps)
It just reads uint16_t from buffer and writes it to second buffer after shifting.
"for capturing raw 10bits data, you need to set RAW16 in ISI , and right shift 4bits to get the correct data."
How to do it, could you tell me which file and which function?
How to do it in gstreamer? Could you send me?
Isn't it possible to make ISI to generate data in proper format?
Hi, Joan,
So far as I know, it is not support RAW in early BSP. Which version started to support RAW?
Do we need to add RAW in mxc_isi_src_formats and mxc_isi_out_formats?
I was thinking if CSC block can be active when output is RAW