How to calculate hsync, vsync start, width, end value in hdmi with 800x600?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to calculate hsync, vsync start, width, end value in hdmi with 800x600?

3,025 Views
yibhan
Contributor III

Hi guys,

I have to set my display resolution with hdmi is 800x600, but i have no idea about some of paramters(hsync start, vsync start). So, I need to calculate these parameter to set up hdmi display for 800x600.

Do you have any reference to help to get values or docs or link?

Labels (2)
0 Kudos
Reply
1 Reply

2,970 Views
joanxie
NXP TechSupport
NXP TechSupport

these parameters are depends on your display, you can refer to the display data sheet, which should include these parameters

0 Kudos
Reply