How to calculate RS-485 data rate ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to calculate RS-485 data rate ?

1,140 Views
Raana
Contributor III

Dear Team,

Right now I'm using i.Mx8qxp based custom board.

There I want to develop the Test application to calculate RS-485 data rate.

I'm new to RS-485.

Can any one guide me to move further?

Is there any command or calculation or algorithm to achieve this?

Thanks in Advance.

Thank You.

Best Regards,

J.P.Raja

0 Kudos
4 Replies

1,060 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

As the linux BSP for i.MX8QXP do not support, so for the RS 485 using you can use the Sensing IO direction Automatically via hardware, don't need to tune software. The follow is used on i.MX6, you can refer to .

RS485.png

0 Kudos

1,060 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which version of BSP are you using?

0 Kudos

1,060 Views
Raana
Contributor III

Hi Rita Wang,

Thanks for your response.

I'm using the "imx-yocto-L4.14.98_2.0.0_ga" version.

Thank You.

Best Regards,

J.P.Raja

0 Kudos

1,060 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can connect two RS-485 module to test the rate.

0 Kudos