How to bypass FlexCAN ID Filter to receive All Extended AND Standard frames on iMX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to bypass FlexCAN ID Filter to receive All Extended AND Standard frames on iMX8

ソリューションへジャンプ
1,355件の閲覧回数
Lornix
Contributor I

As the title says, i want to set FlexCAN peripheral to receive ALL frames (Standard AND Extended), without any filter

It seems to me that it's impossibile to do this by FIFO mode, because it is mandatory to specify IDE bit

Witch is the "right" way to do so?

Thank you

0 件の賞賛
返信
1 解決策
1,306件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

I do not actually know which i.MX8 are you using or which core, either Cortex-A or Cortex-M, but you may refer to this community thread for an example for Cortex-M
https://community.nxp.com/t5/i-MX-Processors/FlexCAN-filter-of-type-quot-Range-quot-in-iMX8-CM7/td-p...

While for Cortex-A you may refer to the following app note:
https://www.nxp.com/webapp/Download?colCode=AN13210
Chapter 4.4.7 Filter the received CAN frames, you may try setting can_mask to 0  so it receives any ID.

Best regards,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,294件の閲覧回数
Lornix
Contributor I

Thank you Aldo,

I am using MIMX8ML8_M7

I'll check your links

0 件の賞賛
返信
1,307件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

I do not actually know which i.MX8 are you using or which core, either Cortex-A or Cortex-M, but you may refer to this community thread for an example for Cortex-M
https://community.nxp.com/t5/i-MX-Processors/FlexCAN-filter-of-type-quot-Range-quot-in-iMX8-CM7/td-p...

While for Cortex-A you may refer to the following app note:
https://www.nxp.com/webapp/Download?colCode=AN13210
Chapter 4.4.7 Filter the received CAN frames, you may try setting can_mask to 0  so it receives any ID.

Best regards,
Aldo.

0 件の賞賛
返信