How to buy camera module for MIMXRT1050-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to buy camera module for MIMXRT1050-EVK

2,564 Views
hiectai
Contributor III

Hi community!

I want to evaluate the camera performance on MIMXRT1050-EVK, but i can not find where to buy camera module.


Could you tell me how to buy camera module for MIMXRT1050-EVK?

Thank you so much.

4 Replies

1,785 Views
mariocenteno
NXP Employee
NXP Employee

Hello,

Camera modules are supplied by:

CompanyHua Tian technology(KunShan) Electronics, CO.,Ltd.

Website: http://gb.htkjks.com/

or you can buy a i.MX RT1060 evk. They include the camera module.

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/mimxrt106...

thanks,

Mario

1,785 Views
steve1
Contributor I

Hello Mario,

Is it possible to buy the module separately or do we have to buy the 1060 evkit? I want to use the 1050 in my application. 

0 Kudos

1,785 Views
BlackNight
NXP Employee
NXP Employee

I ordered a cameras from Aliexpress, see Using Camera Modules with NXP i.MX RT10xx EVK | MCU on Eclipse 

I hope this helps,

Erich

0 Kudos

1,785 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi タイ チャン,

Here is the camera we are using for i.MX RT1050:
EVK designed with both MT9M114(720P) and MT7725(VGA).
And SDK next release will have MT9M114 support by default.

You can find more information here:

i.MX rt1050 camera example 


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------