How to burn QNX SDP 8.0 image into IMX8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to burn QNX SDP 8.0 image into IMX8QM

601件の閲覧回数
JustinLu
Contributor I

Hi,

I have already used Momentics to compile the QNX SDP 8.0 BSP for the i.MX8QM platform.

The following files were generated:

ipl-imx8qm-cpu-mek_b0.imx
ipl-imx8qm-cpu-mek_flash_b0.imx
qnx-ifs-cpu-mek

I used the uuu tool to flash the bootloader and the QNX-IFS image with the following command:

sudo uuu -b sd ipl-imx8qm-cpu-mek_flash_b0.imx qnx-ifs-cpu-mek

The UART output indicates that the IPL is ready, but I am unable to flash the image.

Welcome to QNX Initial Program Loader for NXP i.MX8QM(Rev B) MEK Board (ARM Cortex-A53/A72)
SCFW build version: 5624, SCFW commit: 6638c032
SECO version: 2.5.6, commit: 6638c032
Command:
Press 'D' for serial download, using the 'sendnto' utility
Press 'M' for eSDC download, IFS filename MUST be 'QNX-IFS'
Press 'E' for eMMC download, IFS filename MUST be 'QNX-IFS'
Press 'F' for NOR flash download, IFS MUST be at 0x100000 offset

What is the correct way to flash the QNX image?

タグ(1)
0 件の賞賛
返信
1 返信

582件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @JustinLu!

Thank you for contacting NXP Support!

 

Unfortunately we don´t have guides for QNX.

 

I recommend to check the QNX Documentation or contact to QNX Support.

 

Best Regards!

Chavira

0 件の賞賛
返信