How to build the MFG uboot for Android 6.0 on imx6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build the MFG uboot for Android 6.0 on imx6?

2,237 Views
alleenwang
Contributor II

Hi all,

I want to build the uboot for MFGTool upgrade.

This uboot for first boot up device, not for writing to eMMC.

example : 

<LIST name="eMMC-Android" desc="Choose eMMC as media">
   <CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx6q%plus%%board%_sd.imx" ifdev="MX6Q">Loading U-boot</CMD>  <--- I want to build this uboot.

I reference the "Manufacturing Tool V2 Linux or Android Firmware Development Guide V2.docx" on MFGTool package.

(android_m6.0.1_2.1.0_tool.tar.gz)

Base on this document, I can't find the mx6q_sabresd_mfg.h on the last version.

So, I think this document was an older version, it only builds the "uboot.bin" not "uboot.imx".

Anyone can help me?

Thanks!!!

BR.

Alleen

Labels (2)
0 Kudos
Reply
2 Replies

1,810 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aleen

it may be useful to check sect.6.2 Manufacturing Tool, MFGTool

attached Yocto Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,810 Views
aravinthkumarja
Senior Contributor II

Hi Allen Wang,

You can use target board uboot on MFG tool also. There is not difference on uboot. Kernel only have difference for MFGTool

Regards,

Aravinth

0 Kudos
Reply