How to build .so file on Android 6.0 source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to build .so file on Android 6.0 source

1,990件の閲覧回数
wangvictor
Contributor III

Hi All,

I'm using iMX6 sabresd and building image for Android 6.0.

Here is my Android.mk.

hardware/ril/ublox_ril/CORE/Android.mk

#
# Copyright 2010 Intrinsyc Software International, Inc. All rights reserved.
#

LOCAL_PATH:= $(call my-dir)

include $(CLEAR_VARS)

LOCAL_SRC_FILES:= \
ND/te_base.cpp \
ND/te.cpp \
ND/systemmanager.cpp \
ND/radio_state.cpp \
silo.cpp \
ND/silo_voice.cpp \
ND/silo_network.cpp \
ND/misc.c \
ND/silo_sim.cpp \
ND/silo_data.cpp \
ND/silo_phonebook.cpp \
ND/silo_sms.cpp \
ND/channel_nd.cpp \
channelbase.cpp \
channel_atcmd.cpp \
channel_data.cpp \
channel_DLC2.cpp \
channel_DLC6.cpp \
channel_DLC8.cpp \
port.cpp \
ND/callbacks.cpp \
ND/file_ops.cpp \
ND/rildmain.cpp \
ND/sync_ops.cpp \
ND/thread_ops.cpp \
ND/ril_result_nd.cpp \
cmdcontext.cpp \
command.cpp \
globals.cpp \
rilchannels.cpp \
response.cpp \
request_info_table.cpp \
thread_manager.cpp \
ND/silo_factory.cpp \
ND/MODEMS/te_inf_u120.cpp \
ND/MODEMS/te_cdma.cpp \
ND/MODEMS/te_modem_toby_R2.cpp \
ND/MODEMS/silo_voice_inf.cpp \
ND/MODEMS/silo_sim_inf.cpp \
ND/MODEMS/silo_sms_inf.cpp \
ND/MODEMS/silo_data_inf.cpp \
ND/MODEMS/silo_network_inf.cpp \
ND/MODEMS/silo_phonebook_inf.cpp

LOCAL_SHARED_LIBRARIES := \
libcutils libutils

#librilutils is required for Android 4.4 and above
ifeq (1,$(strip $(shell expr $(PLATFORM_VERSION) \>= 4.4)))
LOCAL_SHARED_LIBRARIES += librilutils
endif

LOCAL_CFLAGS = -DRIL_RADIO_RESILIENCE

LOCAL_CFLAGS += -DDEBUG
#LOCAL_CFLAGS += -DRIL_ENABLE_CHANNEL_DATA1
LOCAL_CFLAGS += -DRIL_ENABLE_SIMTK
LOCAL_CFLAGS += -DUSE_STK_RAW_MODE
#LOCAL_CFLAGS += -DRIL_JB_RAT_REMAPPING

#PLATFORM_VERSION is checked at compile-time and the corresponding flag is defined
# Setting flags for android jellybeans (4.1 - 4.3)
ifeq (1,$(strip $(shell expr $(PLATFORM_VERSION) \>= 4.1)))
ifeq (1,$(strip $(shell expr $(PLATFORM_VERSION) \< 4.4)))
LOCAL_CFLAGS += -DANDROID_JB
endif
endif

# Setting flags for android kitkat (4.4.x)
ifneq ($(shell echo '$(PLATFORM_VERSION)' | grep '^4.4'),)
LOCAL_CFLAGS += -DANDROID_KK
endif

# Setting flags for android lollipop (5.x.x)
ifneq ($(shell echo '$(PLATFORM_VERSION)' | grep '^5'),)
LOCAL_CFLAGS += -DANDROID_LP
endif

# Setting flags for android marshmallow (6.x.x)
ifneq ($(shell echo '$(PLATFORM_VERSION)' | grep '^6'),)
LOCAL_CFLAGS += -DANDROID_MM
$(warning "winmate victor the value of LOCAL_PATH is $(LOCAL_MODULE)")
endif

#include this if you want a TIMEBOMB.
#LOCAL_CFLAGS += -DTIMEBOMB

LOCAL_C_INCLUDES := \
$(KERNEL_HEADERS) \
$(LOCAL_PATH)/ND \
$(LOCAL_PATH)/ND/MODEMS \
$(LOCAL_PATH)/MODEMS \
$(LOCAL_PATH)/../INC \
$(LOCAL_PATH)/../OEM/ND \
$(LOCAL_PATH)/../UTIL/ND


#build shared library
LOCAL_PRELINK_MODULE := false
LOCAL_STRIP_MODULE := true
LOCAL_SHARED_LIBRARIES += \
librapid-ril-util \
librapid-ril-oem
#LOCAL_LDLIBS += -lpthread
#Modification required by Android 4.3
LOCAL_LDLIBS += -llog
LOCAL_CFLAGS += -DRIL_SHLIB -Os
LOCAL_MODULE:= librapid-ril-core
$(warning "winmate victor the value of LOCAL_PATH is $(LOCAL_MODULE)")
LOCAL_MODULE_TAGS:= optional
include $(BUILD_SHARED_LIBRARY)

And it suppose to build the librapid-ril-core.so out and put it under folder out/.

But I can't build any.

The weird thing is when I compiling there is no error came out.

I'm sure that computer did run into this file cause I had print the log.

Why can't I build the librapid-ril-core.so out?

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

1,703件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Firstly your .mk file  should be included by your last dir.

Secondly, you should add in librapid PRODUCT_PACKAGE which is in  device/fsl/imx6/imx6.mk

0 件の賞賛
返信

1,703件の閲覧回数
wangvictor
Contributor III

I add it in this file device/fsl/FM100A/BoardConfig.mk

.
.
.

RIL_COM_INTERFACE := usb
PRODUCT_PACKAGES += librapid-ril-core \
gsm0710muxd \
chat

PRODUCT_PACKAGES += rild
PRODUCT_COPY_FILES += \
system/core/rootdir/init.usb.rc:root/init.usb.rc \
system/core/rootdir/init.trace.rc:root/init.trace.rc \
build/target/product/rootdir/etc/init.gprs-pppd:system/bin/init.gprs-pppd \
build/target/product/rootdir/etc/init_data_android_6:system/bin/init_data \
build/target/product/rootdir/etc/stop_data_android_6:system/bin/stop_data \
build/target/product/rootdir/etc/ppp/chap-secrets:system/etc/ppp/chap-secrets \
build/target/product/rootdir/etc/ppp/ip-down:system/bin/ip-down \
build/target/product/rootdir/etc/ppp/ip-up:system/bin/ip-up \
build/target/product/rootdir/etc/ppp/chap-secrets:system/etc/ppp/pap-secrets \
build/target/product/rootdir/etc/ppp/stop_pppd:system/bin/stop_pppd \
build/target/product/rootdir/etc/uril/repository.txt:system/etc/uril/repository.txt \
build/target/product/rootdir/etc/uril-repo.sh:system/bin/uril-repo.sh \
build/target/product/rootdir/etc/static_apn:system/bin/static_apn

PRODUCT_COPY_FILES += \
build/target/product/rootdir/etc/stop_muxd:system/bin/stop_muxd \
build/target/product/rootdir/etc/ppp/cdma-chat-isp:/system/etc/ppp/cdma-chat-isp \
build/target/product/rootdir/etc/ppp/peers/cdma-usb-gprs1:system/etc/ppp/peers/cdma-usb-gprs1 \
build/target/product/rootdir/etc/ppp/chat-isp1:/system/etc/ppp/chat-isp1 \
build/target/product/rootdir/etc/ppp/chat-isp2:/system/etc/ppp/chat-isp2 \
build/target/product/rootdir/etc/ppp/chat-isp3:/system/etc/ppp/chat-isp3 \
build/target/product/rootdir/etc/ppp/chat-isp4:/system/etc/ppp/chat-isp4 \
build/target/product/rootdir/etc/ppp/peers/usb-gprs1:system/etc/ppp/peers/usb-gprs1 \
build/target/product/rootdir/etc/ppp/peers/usb-gprs2:system/etc/ppp/peers/usb-gprs2 \
build/target/product/rootdir/etc/ppp/peers/usb-gprs3:system/etc/ppp/peers/usb-gprs3 \
build/target/product/rootdir/etc/ppp/peers/usb-gprs4:system/etc/ppp/peers/usb-gprs4

I did have add the PRODUCT_PACKAGES and I also check that compiler did run this file.

Any help?

Thanks in Advanced!

0 件の賞賛
返信

1,703件の閲覧回数
wangvictor
Contributor III

jamesbone

First: What did you mean included by my last dir?

Second : I've check the PRODUCT_PACKAGE is already write in the device/fsl/FM100A/BoardConfig.mk which is my customize file.

0 件の賞賛
返信