How to build imx-boot-imx8qxpmek-sd.bin-flash as in the pre-built image?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build imx-boot-imx8qxpmek-sd.bin-flash as in the pre-built image?

3,347 Views
fei_4_xu
Contributor III

Hi,

I'm using a imx8qxp-mek board with the pre-built images (L4.14.98_2.0.0_ga_images_MX8QXPMEK.zip). I can use uuu.exe to download the image.

 

From the pre-built zip file, I can find a uuu.auto file, which has a line like this:

SDPS: boot -f imx-boot-imx8qxpmek-sd.bin-flash

 

But after a successful bitbake, I can only find  imx-boot-imx8qxpmek-sd.bin-flash_spl and imx-boot-imx8qxpmek-sd.bin-flash_linux_m4 in my tmp/deploy/images/imx8qxpmek folder, but not imx-boot-imx8qxpmek-sd.bin-flash.

 

So my question is: how to build the .bin-flash file as in the pre-build image in yocto?

0 Kudos
Reply
2 Replies

2,519 Views
josephzhou1
Contributor V

if u make it only core -a  img

 

make SOC=iMX8QM flash

 

then the file name will be 

SDPS: boot -f imx-boot-imx8qxpmek-sd.bin-flash
Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 Kudos
Reply

3,328 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,


This process is usually describe in our i.MX Linux User's Guide, section 4.5.13 How to build imx-boot image by using imx-mkimage.

I also find this guide quite useful, please take a look as well:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootab...

 

Hope this helps,
Regards,
Aldo.

0 Kudos
Reply