Hello all.
I have question about OpenCV in Yocto project (git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga) .
When I use Yocto project to porting i.MX6 quad board, I cannot use Videowriter in OpenCV.
So I want to update Yocto project's OpenCV library.
First, I downloaded and built OpenCV 2.4.11 (It is same version with Yocto project's OpenCV)
As you know, 1) Yocto project's OpenCV and 2) another OpenCV what I downloaded consist of different file structure such as 'toolchain.cmake'.
How can I update OpenCV from 2) to 1) in Yocto project?
Or Can I use 'cmake' command to build 2) OpenCV to Yocto project?
I need your help.
Thanks,
BR.
Hi Yongdeuk,
you can just add
IMAGE_INSTALL_append " \
cmake \
You can run bitbake -s | grep cmake to see the avaliable options.
Thanks for replying, Bio_TICFSL!
IMAGE_INSTALL_append " \
cmake \
What you said is about 'local.conf', right?
But, when Yocto project image(fsl-image-gui or fsl-image-qt5) built, OpenCV 2.4.11 is included without any options.
Please tell me details about your comments :smileyhappy:
Thanks,
BR.