How to build core-image-rt on imx6qpsabresd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to build core-image-rt on imx6qpsabresd

1,272件の閲覧回数
enriqueencarnac
Contributor II

Hi,

I am trying to build “core-image-rt” for a imx6qpsabresd board using bitbake, but I am getting a message Nothing PROVIDES   ‘linux-yocto-rt’

I have included the PREFERRED_PROVIDER_virtual/kernel = “linux-yocto-rt” in my local.conf file, is that correct?

Or should I be somehow using linux-fslc-mx6-rt  somewhere?

Could you point me to some documentation/examples that build systems using pthreads and timers?

ラベル(1)
0 件の賞賛
返信
1 返信

1,029件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Enrique Encarnación,

You are not specifying which BSP you are using but the problem in this case may be that while core-image-rt is available as part of the Open Embedded and thus is a valid image name, the i.MX6QP BSP does not support Linux Real Time. You would need to add the required dependencies and adjustments in order to build a Linux Real Time image for the i.MX6QP.

Regards,

0 件の賞賛
返信