Hi,
I'm trying to build u-boot and load it into my mx6ul evk using imx_usb from Boundary Devices. The output from imx_usb states "No dcd table", so I guess my problem is the missing DCD. I'm able to successfully load the u-boot-imx6ulevk_sd.imx file from NXP's prebuilds (L4.1.15_1.1.0_ga_images_MX6ULEVK), so I'm guessing the imx_usb tool is working.
Am I using the correct u-boot repository (and branch)?
u-boot repo (master branch): git://git.denx.de/u-boot.git
I'm building u-boot.imx with (our own crossng cross compiler):
export BUILD_DIR=$PWD/build
export ARCH=arm
export CROSS_COMPILE=arm-unknown-linux-gnueabihf-
export PATH=$PATH:/usr/compiler/arm-unknown-linux-gnueabihf/bin
make O=build mrproper
make O=build mx6ul_14x14_evk_defconfig
make O=build u-boot.imx
Output from imx_usb:
./imx_usb ../u-boot/build/u-boot.imx config file <./imx_usb.conf> vid=0x066f pid=0x3780 file_name=mx23_usb_work.conf vid=0x15a2 pid=0x004f file_name=mx28_usb_work.conf vid=0x15a2 pid=0x0052 file_name=mx50_usb_work.conf vid=0x15a2 pid=0x0054 file_name=mx6_usb_work.conf vid=0x15a2 pid=0x0061 file_name=mx6_usb_work.conf vid=0x15a2 pid=0x0063 file_name=mx6_usb_work.conf vid=0x15a2 pid=0x0071 file_name=mx6_usb_work.conf vid=0x15a2 pid=0x007d file_name=mx6_usb_work.conf vid=0x15a2 pid=0x0076 file_name=mx7_usb_work.conf vid=0x15a2 pid=0x0041 file_name=mx51_usb_work.conf vid=0x15a2 pid=0x004e file_name=mx53_usb_work.conf vid=0x15a2 pid=0x006a file_name=vybrid_usb_work.conf vid=0x066f pid=0x37ff file_name=linux_gadget.conf config file <./mx6_usb_work.conf> parse ./mx6_usb_work.conf 15a2:007d(mx6_qsb) bConfigurationValue =1 Interface 0 claimed HAB security state: development mode (0x56787856) == work item filename ../u-boot/build/u-boot.imx load_size 0 bytes load_addr 0x00000000 dcd 1 clear_dcd 0 plug 1 jump_mode 2 jump_addr 0x00000000 == end work item No dcd table, barker=402000d1 loading binary file(../u-boot/build/u-boot.imx) to 877ff400, skip=0, fsize=50c00 type=aa out err=-7, last_trans=0 cnt=0x4000 max=0x400 transferSize=0x0 retry=0 out err=-7, last_trans=0 cnt=0x4000 max=0x200 transferSize=0x0 retry=1 out err=-7, last_trans=0 cnt=0x4000 max=0x100 transferSize=0x0 retry=2 out err=-7, last_trans=0 cnt=0x4000 max=0x80 transferSize=0x0 retry=3 out err=-7, last_trans=0 cnt=0x4000 max=0x40 transferSize=0x0 retry=4 out err=-7, last_trans=0 cnt=0x4000 max=0x20 transferSize=0x0 retry=5 out err=-7, last_trans=0 cnt=0x4000 max=0x10 transferSize=0x0 retry=6 out err=-7, last_trans=0 cnt=0x4000 max=0x8 transferSize=0x0 retry=7 out err=-7, last_trans=0 cnt=0x4000 max=0x10 transferSize=0x0 retry=8 out err=-7, last_trans=0 cnt=0x4000 max=0x8 transferSize=0x0 retry=9 out err=-7, last_trans=0 cnt=0x4000 max=0x10 transferSize=0x0 retry=10 Giving up HAB security state: development mode (0x00000000)
imx_usb source:
GitHub - boundarydevices/imx_usb_loader: Usb loader for imx51/53/6x
已解决! 转到解答。
I found the right repo: uboot-imx.git - Freescale i.MX u-boot Tree
I chose branch imx_v2015.04_4.1.15_1.0.0_ga
I also found a description: Building U-boot
I found the right repo: uboot-imx.git - Freescale i.MX u-boot Tree
I chose branch imx_v2015.04_4.1.15_1.0.0_ga
I also found a description: Building U-boot