How to build Mfg firmware images to flash to eMMC in iMX6SL for Marshmallo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to build Mfg firmware images to flash to eMMC in iMX6SL for Marshmallo

4,748 次查看
jansirani
Contributor III

Hai,

we designed a custom board same as iMX6SLEVK.

In this board both sdcard boot and eMMC boot are using sd2 interface same as iMX6SLEVK design .

we successfully compiled and flashed Marshmallo images to the sdcard using Mfgtools and the board is booting without any issues from sdcard.

Now we want to flash images to the eMMC .we added changes to be required for eMMC in u-boot and in kernel.

for Normal images we used "make mx6slevkandroid_defconfig" and "make imx_v7_android_defconfig" and compiled whole filesystem and we got normal images in the myandroid/out/...../evk_6sl folder.

Then,

for Mfg images we used the following commands to build uboot.bin & zImage:

uboot:

make mx6slevk_defconfig

kernel:

make imx_v7_mfg_defconfig

Replaced only uboot.bin & zImage in the Mfgtools/......./firmware/  folder

and Replaced respective normal images in the  Mfgtools/......./files/android/evk  folder .

when we run the mfgtool.exe, it is getting stop at "starting kernel"

i.e:

"
U-Boot 2015.04-dirty (Dec 16 2016 - 09:52:10)

CPU:   Freescale i.MX6SL rev1.2 at 792 MHz
CPU:   Temperature 42 C
Reset cause: POR
Board: MX6SLEVK
I2C:   ready
DRAM:  1 GiB
PMIC:  PFUZE100 ID=0x10
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2             
*** Warning - bad CRC, using default environment

In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc1(part 0) is current device
Net:   Phy 0 not found
PHY reset timed out
FEC [PRIME]
Error: FEC address not set.

Boot from USB for mfgtools
Use default environment for                              mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot:  0
Kernel image @ 0x80800000 [ 0x000000 - 0x5a6bd8 ]
## Loading init Ramdisk from Legacy Image at 83800000 ...
   Image Name:   fsl-image-mfgtool-initramfs-imx6
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    7565864 Bytes = 7.2 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
   Booting using the fdt blob at 0x83000000
   Using Device Tree in place at 83000000, end 8300bf7a
switch to ldo_bypass mode!

Starting kernel ...

"

Please tell us how to solve this issue.

标签 (5)
0 项奖励
回复
5 回复数

3,523 次查看
zhihetu
Contributor I
Hi Jansi,

Do you fix this problem? I am facing the same issue.


0 项奖励
回复

3,523 次查看
jansirani
Contributor III

Hai zhihetu

we slove the issue.now we are able to flash images to eMMC in Marshmallo.

To compile Mfg firmware, please download the yocto environment and download  uboot , kernel and fsl-intiramfs using bitbake and use the compiled mfg images for Android flashing using Mfgtools.

0 项奖励
回复

3,522 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jansi

also please check fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot

under ../firmware/  folder, for commands refer to attached Yocto Guide

sect.6.2 Manufacturing Tool.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,522 次查看
jansirani
Contributor III

Hai igorpadykov

According to this yocto user guide, we have to use " bitbake fsl-image-mfgtool-initramfs"

but if we execute this command in myandroid/ , it is giving "bitbake: command not found".

Please guide us how to compile the fsl-image-mfgtool-initramfs in Android .

Thanks & Regards,
D.Jansirani

0 项奖励
回复

3,522 次查看
igorpadykov
NXP Employee
NXP Employee

refer to Manufacturing Tool V2 Linux or Android Firmware Development Guide V2.docx

in mfg tools /Document folder.

Best regards
igor

0 项奖励
回复