How to build Chromium with X11?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to build Chromium with X11?

4,645件の閲覧回数
wangvictor
Contributor III

Hi All,

I wanna build Chromium with X11.

I do it with this command `bitbake chromium`.

And It will give me this error message.

ERROR: No recipes available for:
/mnt/raid115/victor/L4.1.15/sources/meta-fsl-arm/browser-layer/recipes-browser/chromium/chromium_40.0.2214.91.bbappend

More details are here.

This is my conf/local.conf

MACHINE ??= 'imx6qsabresd'
DISTRO ?= 'poky'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES = "debug-tweaks"
USER_CLASSES ?= "buildstats image-mklibs"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS = "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
STOPTASKS,/tmp,100M,100K \
ABORT,${TMPDIR},100M,1K \
ABORT,${DL_DIR},100M,1K \
ABORT,${SSTATE_DIR},100M,1K \
ABORT,/tmp,10M,1K"
PACKAGECONFIG_append_pn-qemu-native = " sdl"
PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"
PACKAGECONFIG_append_pn-qtmultimedia = " gstreamer alsa"
ASSUME_PROVIDED += "libsdl-native"
CONF_VERSION = "1"

DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = "1"

This is my conf/bblayers.conf

LCONF_VERSION = "6"

BBPATH = "${TOPDIR}"
BSPDIR := "${@os.path.abspath(os.path.dirname(d.getVar('FILE', True)) + '/../..')}"

BBFILES ?= ""
BBLAYERS = " \
${BSPDIR}/sources/poky/meta \
${BSPDIR}/sources/poky/meta-yocto \
\
${BSPDIR}/sources/meta-openembedded/meta-oe \
${BSPDIR}/sources/meta-openembedded/meta-multimedia \
\
${BSPDIR}/sources/meta-fsl-arm \
${BSPDIR}/sources/meta-fsl-arm-extra \
${BSPDIR}/sources/meta-fsl-demos \
${BSPDIR}/sources/meta-browser \
"

How to solve this problem?

Thank in Advanced!

ラベル(5)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,675件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the link to check if you install the chromium correct or not

https://community.nxp.com/message/864498 

0 件の賞賛
返信

2,675件の閲覧回数
wangvictor
Contributor III

I've fond the problem that I for got to do DISTRO.

0 件の賞賛
返信