I have configured u-boot to use the eMMC device as the default for boot and for the environment save.
I am using yocto 1.6.2 with everything on the default settings except for adding an emmc u-boot configuration.
Everything boots just fine with no SD Card since the eMMC always enumerates as /dev/mmcblk0
However, if there is an SD Card present during boot the eMMC does not enumerate as /dev/mmcblk0 and the Kernel startup crashes because /dev/mmcblk0p2 no longer contains the root filesystem...
So, How do I get the eMMC to always enumerate first, or always enumerate to the same device as the Kernel boots?
Or is there a different question/answer that gets me to the same effect?
解決済! 解決策の投稿を見る。
Hi Steve,
Good job !
All operations of devices are in .dtb file, you don't need to modify .c file, so your operation is correct .
Regards,
Weidong
Hello Steve,
You can resolve the problem by adjusting the registration sequence of uSDHC device in BSP file. For example, if uSDHC4 ( eMMC connected) is firstly registered, the device will be /dev/mmcblk0, if SD card is connected to uSHDC3 port, second uSDHC device will be registered as /dev/mmcblk1 .....
Regards,
Weidong
Thanks very much! In the interest of making sure I am solving this in the best way, and the way you intended, I want to clarify how I have taken your suggestion:
Device enumeration, in this case, is done whilst parsing the device tree binary (registration is not from a board.c file)
Therefore, I must reorder the declaration of sdhc4 in the device tree to be the first sdhc device probed; we know that sdhc4 will always be found, after all, on the iMX6qSabreSD board.
To do this I have patched the file imx6qdl.dtsi putting "usdhc4: usdhc@0219c000 {...}" before "usdhc1: usdhc@02190000 {...}"
I confirmed the ordering in the dtb by decompiling back into a flat dts and looking for "0219c000" which is now the first usdhc device.
This has worked, I can boot the board now from eMMC with or without an SD Card in either slot.
This was done modifying the device tree by applying a patch locally at build time, there is no Kernel code change.
Was this your intended interpretation?
Hi Steve,
Good job !
All operations of devices are in .dtb file, you don't need to modify .c file, so your operation is correct .
Regards,
Weidong