Hi There,
We have a custom board that is similar to the imx6q sabresd (+NAND flash) that we are working on porting the new Yocto BSP to. What works so far
1. Booting LTIB BSP from SD card and NAND Flash
2. Booting Yocto BSP from SD card (by modifying mx6qsabresd.h & mx6qsabre_common.h)
3. Reading & Writing NAND Flash in Yocto u-boot (2013.04)
However, when attempting to boot the Yocto U-boot from NAND flash there is no bootloader console output. The same binary (but w/o the header - u-boot.imx) written to the SD card (with the 0x400 offset) works OK. I know one needs to modify uboot to have the environment read from the nand-flash, however its my impression that at the very minimum there should be some console output using the same uboot binary. Which is where I might be mistaken. Are there any other modifications needed ? I use the following command to program uboot to Flash.
kobs-ng init -v --chip_0_device_path=/dev/mtd0 u-boot.bin
Programming my LTIB-based uboot using this works OK, so that narrows down the problem to the actual content of the new Yocto u-boot.bin. Hexdumping the mtd0 partition reveals some differences in the first few hundred bytes, but I'm not sure if its significant
@ubuntu:/project/yocto/build1$ hexdump -C ltib_uboot -n 1000
00000000 00 00 67 fb ff ff 46 43 42 20 00 00 00 01 50 3c |..g...FCB ....P<|
00000010 19 06 00 00 00 00 00 08 00 00 40 08 00 00 40 00 |..........@...@.|
00000020 00 00 00 00 00 00 00 00 00 00 00 00 00 00 04 00 |................|
00000030 00 00 00 02 00 00 00 02 00 00 04 00 00 00 0a 00 |................|
00000040 00 00 03 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000050 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000060 00 00 00 00 00 00 00 00 00 00 00 02 00 00 00 05 |................|
00000070 00 00 b9 00 00 00 b9 00 00 00 00 01 00 00 cf 07 |................|
00000080 00 00 00 00 00 00 00 08 00 00 00 00 00 00 00 00 |................|
00000090 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
*
00000200 1c 0f 17 1f 05 00 00 00 00 00 19 00 00 15 19 00 |................|
00000210 00 15 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000220 00 13 00 00 00 00 16 00 00 00 16 00 00 13 00 00 |................|
00000230 00 0f 00 00 00 0a 00 00 00 00 00 00 00 00 00 00 |................|
00000240 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000250 00 00 00 00 00 00 00 00 00 00 00 00 00 00 16 00 |................|
00000260 00 00 0f 00 00 16 00 00 00 16 00 00 00 00 1c 00 |................|
00000270 00 1b 19 00 00 00 00 00 00 00 19 00 00 00 00 00 |................|
00000280 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
@ubuntu:/project/yocto/build1$ hexdump -C uboot_yocto -n 1000
00000000 00 00 d3 fc ff ff 46 43 42 20 00 00 00 01 50 3c |......FCB ....P<|
00000010 19 06 00 00 00 00 00 08 00 00 40 08 00 00 40 00 |..........@...@.|
00000020 00 00 00 00 00 00 00 00 00 00 00 00 00 00 04 00 |................|
00000030 00 00 00 02 00 00 00 02 00 00 04 00 00 00 0a 00 |................|
00000040 00 00 03 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000050 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000060 00 00 00 00 00 00 00 00 00 00 00 02 00 00 00 05 |................|
00000070 00 00 02 01 00 00 02 01 00 00 00 01 00 00 cf 07 |................|
00000080 00 00 00 00 00 00 00 08 00 00 00 00 00 00 00 00 |................|
00000090 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
*
00000200 1c 0f 17 1f 05 00 00 00 00 00 19 00 00 15 19 00 |................|
00000210 00 15 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000220 00 13 00 00 00 00 16 00 00 00 16 00 00 13 00 00 |................|
00000230 00 0f 00 00 00 0a 00 00 00 00 00 00 00 00 00 00 |................|
00000240 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000250 00 00 00 00 00 00 00 00 00 00 00 00 00 00 16 00 |................|
00000260 00 00 0f 00 00 16 1c 00 00 16 1c 00 00 00 1c 00 |................|
00000270 00 1b 19 00 00 00 00 00 00 00 19 00 00 00 00 00 |................|
00000280 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
*
000003e8
Also, performing a "nand dump 0" in the LTIB u-boot shows the same data as in the new Yocto u-boot. That proves that the Yocto u-boot can read the Flash OK.
Any hints on what the problem could be would be appreciated
Thanks,
/Otto
andrewk