Hi
I have i.MX53 QSB. We want to boot from Trensend MMC Plus card.
I tried to follow i.MX53 start linux user's guide. It doesn't work.
It will show information as below.
Would someone please help that?
Thanks
u-boot.bin and uImage file comes from /ltib/rootfs/boot/
U-Boot 2009.08 (Dec 14 2011 - 11:35:51)
CPU:   Freescale i.MX53 family 2.0V at 1000 MHz
mx53 pll1: 1000MHz
mx53 pll2: 400MHz
mx53 pll3: 216MHz
mx53 pll4: 455MHz
ipg clock     : 66666666Hz
ipg per clock : 33333333Hz
uart clock    : 21600000Hz
cspi clock    : 54000000Hz
ahb clock     : 133333333Hz
axi_a clock   : 400000000Hz
axi_b clock   : 200000000Hz
emi_slow clock: 133333333Hz
ddr clock     : 400000000Hz
esdhc1 clock  : 80000000Hz
esdhc2 clock  : 80000000Hz
esdhc3 clock  : 80000000Hz
esdhc4 clock  : 80000000Hz
nfc clock     : 26666666Hz
Board: MX53-LOCO 1.0
Boot Reason: [POR]
Boot Device: MMC
I2C:   ready
DRAM:   1 GB
MMC:   FSL_ESDHC: 0, FSL_ESDHC: 1
*** Warning - bad CRC or MMC, using default environment
In:    serial
Out:   serial
Err:   serial
Net:   got MAC address from IIM: 00:04:9f:01:b4:f9
FEC0 [PRIME]
Hit any key to stop autoboot:  0
MX53-LOCO U-Boot > mmcinfo
Card did not respond to voltage select!
MMC card init failed!
MX53-LOCO U-Boot >
As far as I know, We place an MMC/SD Card in the slot at the down-side, that is mmcblk0pX. Change it, I would say to you to check this again.
Try this and see.
If the above does not work, Check your env variables again.
Hi Krishna
Much appreciate your help.
I tried to use variable "mmcblk1p2". It doesn't work.
The result is
"Wrong Image Format for bootm command
ERROR: can't get kernel image!"
By the way, I use Transcend 4GB MMCplus card.
Would you please recommend 4GB MMC card?
Thanks
 
 Krishna Pavan said:
Hi Henry,
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p2 rootwait ${vga}'
Check the above variable, mmcblk1p2, it should be mmcblk0px.
Hi Henry,
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p2 rootwait ${vga}'
Check the above variable, mmcblk1p2, it should be mmcblk0px.
HI Krishna
Thanks.
I also do it.
But the result is
"Wrong Image Format for bootm command
ERROR: can't get kernel image!"
What I flash the MMC is
1.Flash U-boot and UIamge from demo image such as
sudo dd if=u-boot-mx53-loco.bin of=/dev/sdc bs=512 && sync && sync
sudo dd if=uImage of=/dev/sdc bs=512 seek=2048 && sync && sync
 
 Krishna Pavan said:
Hi Henry,
sudo dd if=u-boot-mx53-loco.bin of=/dev/mmcblk0 bs=512 && sync && sync
sudo dd if=uImage of=/dev/mmcblk0 bs=512 seek=2048 && sync && sync
Instead of /dev/mmcblk0, you should use the device that appears in fdisk -l command.
Regards Krishna Pavan
Hi Henry,
sudo dd if=u-boot-mx53-loco.bin of=/dev/mmcblk0 bs=512 && sync && sync
sudo dd if=uImage of=/dev/mmcblk0 bs=512 seek=2048 && sync && sync
Instead of /dev/mmcblk0, you should use the device that appears in fdisk -l command.
Regards Krishna Pavan
Hi Alan
Much appreciate your help
Sorry to late reply.
I have tested the environment variable such as "i.MX53 START Linux User's Guide " Sec.8.2 Run the Image from MMC/SD
and your seggestion.
The result will come out
"MMC read: dev # 1, block # 2048, count 6144 partition # 0 ...
6144 blocks read: OK
Wrong Image Format for bootm command
ERROR: can't get kernel image!"
Here is my environment variable and console message.
Would you please kindly help it?
Thanks
1.Flash U-boot and UIamge from demo image such as
sudo dd if=u-boot-mx53-loco.bin of=/dev/mmcblk0 bs=512 && sync && sync
sudo dd if=uImage of=/dev/mmcblk0 bs=512 seek=2048 && sync && sync
2.Environment variable setting
setenv bootargs_base 'setenv bootargs console=ttymxc0,115200'
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p2 rootwait ${vga}'
setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc read 1 ${loadaddr} 0x800 0x1800;bootm'
setenv bootcmd 'run bootcmd_mmc'
saveenv
run bootcmd
The console message comes out:
MX53-LOCO U-Boot > setenv bootargs_base 'setenv bootargs console=ttymxc0,115200'
MX53-LOCO U-Boot > setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mm
cblk1p2 rootwait ${vga}'
MX53-LOCO U-Boot > setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc read 1
 ${loadaddr} 0x800 0x1800;bootm'
MX53-LOCO U-Boot > setenv bootcmd 'run bootcmd_mmc'
MX53-LOCO U-Boot > saveenv
Saving Environment to MMC...
Writing to MMC(1)... done
MX53-LOCO U-Boot > run bootcmd
MMC read: dev # 1, block # 2048, count 6144 partition # 0 ...
6144 blocks read: OK
Wrong Image Format for bootm command
ERROR: can't get kernel image!
MX53-LOCO U-Boot >
 Alan Levy said:
I can't see why you would want the mmc write command. Having done it once however you'll have to re-install the operating system onto the SD card before proceeding. As for the environment, I would have expected something like:
setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait ${vga}
Hi Alan
Thanks for help.
I will try the environment configuration.
Thanks
Henry
 
 Alan Levy said:
I can't see why you would want the mmc write command. Having done it once however you'll have to re-install the operating system onto the SD card before proceeding. As for the environment, I would have expected something like:
setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait ${vga}
I can't see why you would want the mmc write command. Having done it once however you'll have to re-install the operating system onto the SD card before proceeding. As for the environment, I would have expected something like:
setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait ${vga}
Hi Alan
Yes.
mmc write command is that I'm trying to make it.
If I didn't have "mmc write" command, would that be OK?
I will tried it.
By the way, does the environment setting be correct?
Much appreciate your great help.
Henry
 
 Alan Levy said:
It appears that you've overwitten the Linux image on the SD card with whatever happened to be in RAM when U-Boot started up. Was that really what you were trying to do with the 'mmc write' command?
It appears that you've overwitten the Linux image on the SD card with whatever happened to be in RAM when U-Boot started up. Was that really what you were trying to do with the 'mmc write' command?
Hi Alan
Thanks for great help.
I follow your suggestion to type mmcinfo 1.
It can read out information as below:
MMC:   FSL_ESDHC: 0, FSL_ESDHC: 1
*** Warning - bad CRC or MMC, using default environment
In:    serial
Out:   serial
Err:   serial
Net:   got MAC address from IIM: 00:04:9f:01:b4:f9
FEC0 [PRIME]
Hit any key to stop autoboot:  0
FEC: enable RMII gasket
PHY indentify @ 0x0 = 0x0007c0f1
*** ERROR: `serverip' not set
Wrong Image Format for bootm command
ERROR: can't get kernel image!
MX53-LOCO U-Boot > mmcinfo
Card did not respond to voltage select!
MMC card init failed!
MX53-LOCO U-Boot > mmcinfo 1
Device: FSL_ESDHC
Manufacturer ID: 1e
OEM: ffff
Name: MMC
Tran Speed: 20000000
Rd Block Len: 512
MMC version 4.0
High Capacity: Yes
Capacity: 4033871872
Bus Width: 8-bit
Boot Partition Size: No boot partition available
I set some environment setting as below
MX53-LOCO U-Boot > setenv bootfile uImage
MX53-LOCO U-Boot > mmc write 1 0x70800000 0x800 0x1800
MMC write: dev # 1, block # 2048, count 6144, partition # 0 ...
6144 blocks written: OK
MX53-LOCO U-Boot > setenv bootargs console=tty,115200 root=/dev/mmcblk1p1 @{vga}
MX53-LOCO U-Boot > setenv boot_mmc 'mmc read 1 ox70800000 0x800 0x1800;bootm 0x7
0800000'
MX53-LOCO U-Boot > setenv bootcmd run boot_mmc
MX53-LOCO U-Boot > saveenv
Saving Environment to MMC...
Writing to MMC(1)... done
MX53-LOCO U-Boot > reset
resetting ...
M
After reset. It will hang.
Would you please help it?
Much appreciate.
Henry
 
 Alan Levy said:
Ah, yes, of course you've got U-boot working already. There are two things I can think of:
1. The full-size card slot is slot 1, not 0. Try:
mmcinfo 1
2. If that doesn't work try turning on switch SW1.8 (if you don't have SW1 fitted, solder a wire between pins 2 and 19).
Ah, yes, of course you've got U-boot working already. There are two things I can think of:
1. The full-size card slot is slot 1, not 0. Try:
mmcinfo 1
2. If that doesn't work try turning on switch SW1.8 (if you don't have SW1 fitted, solder a wire between pins 2 and 19).
Hi Alan
Thanks.
I have modify hardware.
But it doesn't work for MMC plus card.
It works for full size SDHC card.
Would you please help that?
Thanks
 
 Alan Levy said:
The QSB is designed to boot from the micro SD card slot and you have to modify the hardware and software if you want to boot it from the full-size SD card slot. There's a separate thread here which explains how to do this.
The QSB is designed to boot from the micro SD card slot and you have to modify the hardware and software if you want to boot it from the full-size SD card slot. There's a separate thread here which explains how to do this.