Hi
I have applied the linux kernel patch and u-boot patch for SPI.
The sf commands are enabled and sf probe detects spi flash.
I want to know the steps to boot from spi.
I am able to boot from sd card and network.
Linux : 2.6.35 kernel version
Board : MCIMX28EVK
SPI Flash :N25Q128
Regards
Parvathy
Solved! Go to Solution.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Parvathy
software patch for i.MX28 SPI boot has been worked out in Freescale Community.
Please refer to this link for detail:
How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Parvathy
software patch for i.MX28 SPI boot has been worked out in Freescale Community.
Please refer to this link for detail:
How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
Hi
I have applied the kernel patch and uboot patch.By using mk_mx28_sd script,I have burned the image to sd card.
sf probe 2:0 detected the flash.
tftp 0x42000000
sf erase 0x100000 0x300000
sf write 0x42000000 0x100000 0x300000
sf read 0x42000000 0x100000 0x300000
I have used the above commands to write and read from spi.
/**********************************************************************************************************************************************************************************************************************/
Debug uart message log
-------------------------------------------------
U-Boot 2009.08 (Oct 07 2014 - 11:12:16)
Freescale i.MX28 family
CPU: 454 MHz
BUS: 151 MHz
EMI: 205 MHz
GPMI: 24 MHz
DRAM: 128 MB
MMC: IMX_SSP_MMC: 0, IMX_SSP_MMC: 1
In: serial
Out: serial
Err: serial
Net: got MAC address from IIM: 00:04:9f:02:b6:94
FEC0
Hit any key to stop autoboot: 0
MX28 U-Boot > printenv
bootargs=console=ttyAM0,115200n8
bootcmd=run bootcmd_net
bootdelay=3
baudrate=115200
ipaddr=192.168.1.103
serverip=192.168.1.101
netmask=255.255.255.0
bootfile="uImage"
loadaddr=0x42000000
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp fec_mac=${ethaddr}
bootcmd_net=run bootargs_nfs; dhcp; bootm
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p3 rw rootwait ip=dhcp fec_mac=${ethaddr}
bootcmd_mmc=run bootargs_mmc; mmc read 0 ${loadaddr} 100 3000; bootm
ethact=FEC0
nfsroot=/home/i.MX28/ltib/ltib/rootfs
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2009.08 (Oct 07 2014 - 11:12:16)
Environment size: 656/130044 bytes
MX28 U-Boot > setenv serverip 192.168.2.114
MX28 U-Boot > saveenv
Saving Environment to MMC...
Writing to MMC(0)... done
MX28 U-Boot > setenv ipaddr 192.168.2.113
MX28 U-Boot > saveenv
Saving Environment to MMC...
Writing to MMC(0)... done
MX28 U-Boot > printenv
bootargs=console=ttyAM0,115200n8
bootcmd=run bootcmd_net
bootdelay=3
baudrate=115200
netmask=255.255.255.0
bootfile="uImage"
loadaddr=0x42000000
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp fec_mac=${ethaddr}
bootcmd_net=run bootargs_nfs; dhcp; bootm
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p3 rw rootwait ip=dhcp fec_mac=${ethaddr}
bootcmd_mmc=run bootargs_mmc; mmc read 0 ${loadaddr} 100 3000; bootm
ethact=FEC0
nfsroot=/home/i.MX28/ltib/ltib/rootfs
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2009.08 (Oct 07 2014 - 11:12:16)
serverip=192.168.2.114
ipaddr=192.168.2.113
Environment size: 656/130044 bytes
MX28 U-Boot > setenv bootargs_spi 'setenv bootargs ${bootargs} root=/dev/mtdblock2 rootfstype=jffs2 rootwait rw ip=none'
MX28 U-Boot > saveenv
Saving Environment to MMC...
Writing to MMC(0)... done
MX28 U-Boot > setenv bootcmd_spi 'run bootargs_spi;sf probe 2:0; sf read ${loadaddr} 0x100000 0x300000;bootm'
MX28 U-Boot > saveenv
Saving Environment to MMC...
Writing to MMC(0)... done
MX28 U-Boot > run
bootargs bootcmd bootdelay baudrate netmask bootfile loadaddr bootargs_nfs
bootcmd_net bootargs_mmc bootcmd_mmc ethact nfsroot stdin stdout stderr ver
serverip ...
MX28 U-Boot > tftp 0x42000000
Using FEC0 device
TFTP from server 192.168.2.114; our IP address is 192.168.2.113
Filename 'uImage'.
Load address: 0x42000000
Loading: FEC: Link is down 7809
T #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#
done
Bytes transferred = 2998040 (2dbf18 hex)
MX28 U-Boot > sf write
No SPI flash selected. Please run `sf probe'
MX28 U-Boot > sf probe 2:0
SF: Detected N25Q128 with page size 256, total 16777216 bytes
16384 KiB N25Q128 at 2:0 is now current device
MX28 U-Boot > sf probe 2:0
SF: Detected N25Q128 with page size 256, total 16777216 bytes
16384 KiB N25Q128 at 2:0 is now current device
MX28 U-Boot > sf erase 0x100000 0x300000
SF: STMicro: Successfully erased 3145728 bytes @ 0x100000
MX28 U-Boot > sf write 0x42000000 0x100000 0x300000
SF: STMicro: Successfully programmed 3145728 bytes @ 0x100000
MX28 U-Boot > sf read 0x42000000 0x100000 0x300000
MX28 U-Boot > run bootcmd_spi
SF: Detected N25Q128 with page size 256, total 16777216 bytes
16384 KiB N25Q128 at 2:0 is now current device
## Booting kernel from Legacy Image at 42000000 ...
Image Name: Linux-2.6.35.3-g779560d-dirty
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2997976 Bytes = 2.9 MB
Load Address: 40008000
Entry Point: 40008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.35.3-g779560d-dirty (dtsuser@dtsmachine) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #19 PREEMPT Wed Oct 1 16:18:52 IST 2014
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: Freescale MX28EVK board
Memory policy: ECC disabled, Data cache writeback
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512
Kernel command line: console=ttyAM0,115200n8 root=/dev/mtdblock2 rootfstype=jffs2 rootwait rw ip=none
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 128MB = 128MB total
Memory: 123432k/123432k available, 7640k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xfde00000 - 0xffe00000 ( 32 MB)
vmalloc : 0xc8800000 - 0xf0000000 ( 632 MB)
lowmem : 0xc0000000 - 0xc8000000 ( 128 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0034000 ( 176 kB)
.text : 0xc0034000 - 0xc05ce000 (5736 kB)
.data : 0xc05ce000 - 0xc06113a0 ( 269 kB)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
RCU-based detection of stalled CPUs is disabled.
Verbose stalled-CPUs detection is disabled.
NR_IRQS:288
Console: colour dummy device 80x30
console [ttyAM0] enabled
Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux: Initializing.
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
regulator: core version 0.5
NET: Registered protocol family 16
regulator: vddd: 800 <--> 1575 mV at 1500 mV fast normal
regulator: vdddbo: 800 <--> 1575 mV fast normal
regulator: vdda: 1500 <--> 2275 mV at 1800 mV fast normal
vddio = 3380000, val=10
regulator: vddio: 2880 <--> 3680 mV at 3380 mV fast normal
regulator: overall_current: fast normal
regulator: vbus5v:
regulator: mxs-duart-1: fast normal
regulator: mxs-bl-1: fast normal
regulator: mxs-i2c-1: fast normal
regulator: mmc_ssp-1: fast normal
regulator: mmc_ssp-2: fast normal
regulator: charger-1: fast normal
regulator: power-test-1: fast normal
regulator: cpufreq-1: fast normal
i.MX IRAM pool: 124 KB@0xc8820000
usb DR wakeup device is registered
IMX usb wakeup probe
audit: cannot initialize inotify handle
bio: create slab <bio-0> at 0
SCSI subsystem initialized
Freescale USB OTG Driver loaded, $Revision: 1.55 $
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Advanced Linux Sound Architecture Driver Version 1.0.23.
Bluetooth: Core ver 2.15
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
NetLabel: Initializing
NetLabel: domain hash size = 128
NetLabel: protocols = UNLABELED CIPSOv4
NetLabel: unlabeled traffic allowed by default
Switching to clocksource mxs clock source
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Bus freq driver module loaded
IMX usb wakeup probe
usb h1 wakeup device is registered
mxs_cpu_init: cpufreq init finished
audit: initializing netlink socket (disabled)
type=2000 audit(0.660:1): initialized
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
msgmni has been set to 241
alg: No test for stdrng (krng)
cryptodev: driver loaded.
Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Console: switching to colour frame buffer device 100x30
mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART
mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0
Found APPUART 3.1.0
mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1
Found APPUART 3.1.0
mxs-auart.2: ttySP2 at MMIO 0x8006e000 (irq = 114) is a mxs-auart.2
Found APPUART 3.1.0
mxs-auart.3: ttySP3 at MMIO 0x80070000 (irq = 115) is a mxs-auart.3
Found APPUART 3.1.0
mxs-auart.4: ttySP4 at MMIO 0x80072000 (irq = 116) is a mxs-auart.4
Found APPUART 3.1.0
brd: module loaded
loop: module loaded
i.MX GPMI NFC
NFC: Version 1, 8-chip GPMI and BCH
gpmi-nfc: probe of gpmi-nfc.0 failed with error 1
mxs-spi mxs-spi.0: Max possible speed 120000 = 120000000/2 kHz
mxs-spi mxs-spi.0: at 0x80014000 mapped to 0xF0014000, irq=84, bus 1, DMA ver_major 4
FEC Ethernet Driver
fec_enet_mii_bus: probed
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci: irq 93, io base 0x80080000
fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.0: irq 92, io base 0x80090000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
mice: PS/2 mouse device common for all mice
input: mxs-kbd as /devices/platform/mxs-kbd.0/input/input0
input: MXS touchscreen as /devices/virtual/input/input1
MXS RTC driver v1.0 hardware v2.3.0
mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
Linux video capture interface: v2.00
mxs-pxp mxs-pxp.0: initialized
mxs watchdog: initialized, heartbeat 19 sec
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCI H4 protocol initialized
Bluetooth: HCI BCSP protocol initialized
Bluetooth: Generic Bluetooth SDIO driver ver 0.1
mxs-mmc: MXS SSP Controller MMC Interface driver
mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 82 ERRIRQ 96
__mxs_reset_block(f0012000): timeout when resetting
mxs-mmc mxs-mmc.1: mmc1: MXS SSP MMC DMAIRQ 83 ERRIRQ 97
dcp dcp.0: DCP crypto enabled.!
usbcore: registered new interface driver hiddev
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
sgtl5000-i2c 0-000a: SGTL5000 revision 17
mmc0: new high speed SDHC card at address e624
mmcblk0: mmc0:e624 SU04G 3.69 GiB
mmcblk0: p1 p2 p3
mxs-spdif mxs-spdif.0: MXS SPDIF Audio Transmitter
No device for codec mxs spdif
No device for DAI mxs spdif
No device for DAI mxs-saif
No device for DAI mxs-spdif
asoc: SGTL5000 <-> mxs-saif mapping ok
Failed to add route LINE_OUT->Ext Spk
asoc: mxs spdif <-> mxs-spdif mapping ok
ALSA device list:
#0: mxs-evk (SGTL5000)
#1: mxs-evk (mxs spdif)
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (1928 buckets, 7712 max)
CONFIG_NF_CT_ACCT is deprecated and will be removed soon. Please use
nf_conntrack.acct=1 kernel parameter, acct=1 nf_conntrack module option or
sysctl net.netfilter.nf_conntrack_acct=1 to enable it.
ctnetlink v0.93: registering with nfnetlink.
xt_time: kernel timezone is -0000
ip_tables: (C) 2000-2006 Netfilter Core Team
ipt_CLUSTERIP: ClusterIP Version 0.8 loaded successfully
arp_tables: (C) 2002 David S. Miller
TCP cubic registered
NET: Registered protocol family 17
Bridge firewalling registered
Ebtables v2.0 registered
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
Bluetooth: L2CAP ver 2.14
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO (Voice Link) ver 0.6
Bluetooth: SCO socket layer initialized
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
802.1Q VLAN Support v1.8 Ben Greear <greearb@candelatech.com>
All bugs added by David S. Miller <davem@redhat.com>
lib80211: common routines for IEEE802.11 drivers
mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 01:19:55 UTC (4795)
Waiting for root device /dev/mtdblock2...
-------------------------------------------------------------------------------------------------------------------------
Not going beyond this.Its waiting for mtdblock2.How to solve this issue?
Regards
Pt
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		From log:
"Kernel command line: console=ttyAM0,115200n8 root=/dev/mtdblock2 rootfstype=jffs2"
where is located your rootfs system , what device ?
~igor
 
					
				
		
Hi
I need to store rootfs system to spi flash.
I am able to store it sd card and successfully booted up from mmc.
I am using tftp to copy the file in the case of spi.
How to copy rootfs system to mtdblock2 to boot from spi?
Regards
Pt
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Parvathy
I think you can boot from sd and check
if spi-nor mtdblock2 is accessible. Then you can
just copy rootfs from sd to spi-nor.
Usually rootfs is big size, do you have sufficient spi-nor
capacity to hold it ?
~igor
 
					
				
		
Hi igorpadykov
I am using N25Q128 spi flash.
SF: Detected N25Q128 with page size 256, total 16777216 bytes
16384 KiB N25Q128 at 2:0 is now current device
16MB. I think rootfs size is big.so spi boot is not possible,right?
Regards
Pt
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		yes I think 16MB is not sufficient for roofs.
You can boot from spi but have rootfs on other device,
for example sd.
~igor
 
					
				
		
Hi
How to reduce the size of rootfs?
Regards
Pt
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		remove unused programs
~igor
 
					
				
		
Hi
How to optimize the size at compiler level? CFLAGS of complier to reduce size.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		 
					
				
		
Hi
I have used mfgtools to program spi. But I am getting the following error.
Log:
Panel A Start <CMD/> type="push" body="mknod class/mtd,mtd0,/dev/mtd0" file="" timeout="10" onError="" text="".
1 - Panel A Finished <CMD/> type="push" body="mknod class/mtd,mtd0,/dev/mtd0" file="" timeout="10" onError="" text="" FAIL code=0xffffffea.
Panel A: Command is not supported by device.,failed to run command: type="push" body="mknod class/mtd,mtd0,/dev/mtd0" file="" timeout="10" onError="" text=""
2 - Panel A Finished processing SPI-NOR (uboot.sb) <LIST/> : FAIL code=-22.
Regards
Pt
 
					
				
		
Hi
Thank you.I will try to do that.
Regards
Pt